Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Slide 44 Slide 45 Slide 46 Slide 47 Slide 48 Slide 49 Slide 50 Slide 51 Slide 52 Slide 53 Slide 54 Slide 55 Slide 56 Slide 57 Product List
PMIC: CP240x LCD Driver Family Slide 8
There are different methods used to drive the ITO segments in order to generate the electrical field across the liquid crystal material: static and multiplexed. The first method and the simplest to understand is the static drive mode which means each ITO segment of the display has only one connection to the controller. All segments are also referenced to a single common. This mode increases the pin count required to drive the display but it is simpler to create the drive waveforms. The example above shows a single alphanumeric character with the listed segment names, 8A, 8B, etc. As each pin connected to these segments is activated, in addition to the backplane/common reference, the field will be generated and the segment will turn “ON.”
PTM Published on: 2011-05-13