Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Slide 44 Slide 45 Slide 46 Slide 47 Slide 48 Slide 49 Slide 50 Slide 51 Slide 52 Slide 53 Slide 54 Slide 55 Slide 56 Slide 57 Product List
PMIC: CP240x LCD Driver Family Slide 14
This page shows the ULP memory map again. In the static mode example, there was only one common and therefore only bit positions 0 and 4 were used. With multiplexing, and in particular the 4 mux mode as shown, all memory locations are use as each bit position is associated with one of the 4 commons. Bit position 0 is associated with COM0, bit position 1 is associated with COM1 and so on. Take a look at segment 8B in the display mapping in the figure on the right for example. This segment is referenced to COM2 and pin 21. Since the LCD controller pin numbers have been set to be the same as the display pin numbers for this example, segment 8B is mapped to bit position 6 at address ULPMEM10. Other multiplexing modes are available such as 3 mux. In this case COM3 bit positions would not be used.
PTM Published on: 2011-05-13