Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Slide 44 Slide 45 Slide 46 Slide 47 Slide 48 Slide 49 Slide 50 Slide 51 Slide 52 Slide 53 Slide 54 Slide 55 Slide 56 Slide 57 Product List
PMIC: CP240x LCD Driver Family Slide 33
Typically, the data on the SDA line must be stable during the “HIGH” period of the clock. Data can change state only when the SCL line is low. There are two conditions (START and STOP) where these requirements are not met. A master node initiates a transfer by issuing a start condition on the bus as shown above and at the completion of the transfer it issues the stop condition. START and STOP conditions are always generated by the bus master. After a START condition, the bus is considered to be busy. The bus becomes idle again after certain time following a STOP condition or after both the SCL and SDA lines remain high for more than the specified idle time.
PTM Published on: 2011-05-13