Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Slide 44 Slide 45 Slide 46 Slide 47 Slide 48 Slide 49 Slide 50 Slide 51 Slide 52 Slide 53 Slide 54 Slide 55 Slide 56 Slide 57 Product List
PMIC: CP240x LCD Driver Family Slide 4
Now let’s take a look at the construction of a typical segmented display. There are several layers that make up the display as shown in the illustration. The first layer is a vertical polarizer that only allows a single axis of light to pass. Following the polarizer is the glass substrate with the Indium Tin Oxide (ITO) segments. The third layer is the actual liquid crystal material used to “twist” the light. The fourth layer is the glass substrate with an ITO film used as the common reference for the ITO segments. After the common there is another polarizer, this time oriented to allow only light waves in the horizontal plane to pass. This is 90 degrees out of phase with the first polarizer. Beyond the polarizer is the light source. This is either a reflective surface to bounce the incoming light through the display or it can be a backlight. All of the layers are transparent and serve a specific function in passing the light through the display.
PTM Published on: 2011-05-13