Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Slide 44 Slide 45 Slide 46 Slide 47 Slide 48 Slide 49 Slide 50 Slide 51 Slide 52 Slide 53 Slide 54 Slide 55 Slide 56 Slide 57 Product List
PMIC: CP240x LCD Driver Family Slide 55
The programming sequence for Timers 0 and 1 is simple. For Timer 1, there is a clock source selection that has to be made and the initial setup should set the desired clock. Both of the timers operate in an up counting mode with auto-reload meaning that once the overflow condition is met the reload value is then loaded into the count registers. Therefore, the starting value in the timer count registers need to be initialized as well as the reload values. Once the register initialization is complete the timers can be started by setting the run control bits.
PTM Published on: 2011-05-13