Slide 1 Slide 2 Slide 3 Slide 4 Slide 5 Slide 6 Slide 7 Slide 8 Slide 9 Slide 10 Slide 11 Slide 12 Slide 13 Slide 14 Slide 15 Slide 16 Slide 17 Slide 18 Slide 19 Slide 20 Slide 21 Slide 22 Slide 23 Slide 24 Slide 25 Slide 26 Slide 27 Slide 28 Slide 29 Slide 30 Slide 31 Slide 32 Slide 33 Slide 34 Slide 35 Slide 36 Slide 37 Slide 38 Slide 39 Slide 40 Slide 41 Slide 42 Slide 43 Slide 44 Slide 45 Slide 46 Slide 47 Slide 48 Slide 49 Slide 50 Slide 51 Slide 52 Slide 53 Slide 54 Slide 55 Slide 56 Slide 57 Product List
PMIC: CP240x LCD Driver Family Slide 57
In summary, the CP240x family of devices are standalone, fixed-function LCD drivers that generate drive signals for static or multiplexed LCDs. They are designed to interface directly to any MCU via a standard SPI or SMBus/I2C interface. The CP2400 and CP2401 48-pin devices can control up to 128 LCD segments while the CP2402 and CP2403 32-pin devices can control up to 64 LCD segments. Most importantly, the CP240x family has been designed with low power in mind - when paired with the C8051F9xx MCUs, the combined solution from Silicon Labs offers one of the industry’s lowest power solutions for LCD applications.
PTM Published on: 2011-05-13