콘텐츠
상위
Controls and Programmable Logic Controllers (PLCs)
PLC structure
Environmental conditions
Connecting to the Network
Popular PLCs choices for small applications
Popular PLC choices for mid size applications
Popular PLC choices for large scale applications
Popular PLC content
Communication Protocols
Popular junction boxes for communications
Popular content for communications
Programming languages for PLCs
Ladder Diagram (LD) / Relay Logic / Ladder Logic
Function Block Diagram (FBD)
Sequential Function Chart (SFC)
Structured Text (ST)
Instruction List (IL)
CODESYS
Other Languages
Popular Programming Content
Movement and Actuators
Motor Control / Electrical motors
Solenoids / Relays / Contactors
Indicators / Alarms
Popular Actuator Content
Robotics
Industrial Sensors
Pressure
Photoelectric
Proximity
Temperature
Distance
Rotational
Force and Load Cells
Popular Industrial Sensor Products
Popular Industrial Sensor Content
Safety
Regulatory Agencies
Safety Integrity Level (SIL)
Performance Level (PL)
Products
Popular Safety Devices
Popular Safety Content
Machine Vision
Barcode Readers
Machine Vision Cameras
2D vs 3D Vision
Popular Machine Vision Products
Popular Machine Vision Content
Conveyor Block Diagram
Circuit Protection and Line Filter
Uninterruptible Power Supply (UPS)
SMPS 24 VDC
Hold up / Buffer
PLC
IO Modules and Relays
Motor Control
Communications Block
Motor
Cameras and Sensors
Interconnect
Automation Resource Center
Industrial automation and control provides efficiency and consistency in factory operations. This is achieved by using controls to run the logic, industrial sensors to monitor the system, and actuators to move product. These systems need to be rugged and maintain high reliability.
Controls and Programmable Logic Controllers (PLCs)
Programmable Logic Controllers (PLCs) are industrial control units that monitor and respond to incoming signals. The signals they receive are based on sensor and process control data. PLCs respond based on algorithms that are programmed in them.
PLCs range in size from a small DIN rail mounted box to a full 19-inch electronic rack and cabinet with accessories and redundant power supplies.
As with all industrial equipment there may be local and national standards depending on where the equipment is deployed so be sure to double check any relevant standards that may apply.
PLC structure
A PLC is a computing platform with external interfaces for inputs and outputs. Unlike a consumer PC (that may only have a few years of total run time and regular reboots) PLCs are purpose designed and built for industrial environments and applications where a 10 year of up time running 24 hours 7 days a week is considered the norm.
Structurally PLCs can be divided into a few broad sections:
- Input - sensor data and communication signals. Inputs can either be analog signals or digital signals.
- Output - process commands and communication signals (to other networked devices or electromechanical devices [such as relays, valves motor drives, or actuators]).
- Processor & Memory - evaluates incoming data and execute the program instructions.
- Power supply – provides the correct voltage, current, and power requirements, for the PLC.
- Application / Programming / Human Machine Interface (HMI) - HMI as the name suggests, allows humans to interact with the PLC easily to check conditions and operating status (of the PLC). As well, the HMI, can be used to update programing of the PLC. HMIs may range from a simple keyboard to a full touchscreen display.
Programmable Logic Controllers or PLCs are the basic controller for industrial systems
Environmental conditions
Due to the industrial environments where PLC most often operate, they are constructed with higher standards then most consumer rated electronic devices. PLCs are required to be consistent and reliable. They are business critical devices. Any downtime with a PLC often results in a material impact to the business operating it.
Key features to endure these environmental conditions typically include:
- Circuit components with high operating temperature ratings (suited for -40°C to +85°C [-40°F to +185°F]).
- Conformal coatings on circuit boards to withstand high humidity and moisture content.
- Dust filters on all fan intakes or passive cooling heat sinks.
- Electrical isolation on I/O ports and surge protection in PLC circuity (to handle unexpected voltage spikes such as when industrial equipment powers up or down).
Connecting to the Network
PLCs often operate as a hub for communications within a factory, and more recently have become a conduit for information back to enterprise systems (residing in the cloud or back at headquarters).
Popular PLCs choices for small applications
These controllers are ideal for a small setups (this includes operations like switching, timing, and basic sequencing). They are compact and cost effective without all the complexity of the more advanced controllers.
Siemens LOGO! 8.4는 개발을 클라우드로 이전하여 Amazon Web Services(AWS)를 통해 액세스할 수 있으며, 추후 더 많은 옵션이 제공될 예정입니다.
RevPi Core S 및 SE Raspberry Pi 기반 IPC
Raspberry Pi Compute Module을 기반으로 하는 KUNBUS의 업데이트된 산업용 PC RevPi Core 버전은 개방형 하드웨어와 소프트웨어로 구성됩니다.
Popular PLC choices for mid size applications
These controllers offer higher I/O capacity, and advanced communication options. Can work for a small to medium applications. These can deliver strong performance without all the complexity.
Crouzet Automation의 Millenium 3으로 어떤 응용 분야에서든지 최신 세대의 논리 컨트롤러에서 가장 최근의 개발 이점을 취하세요!
Phoenix Contact의 PLCnext는 자동화의 미래를 변화시킬 방식으로 PLC의 사용을 확장하고 있는 최첨단 디지털 에코 시스템입니다.
WAGO의 고성능 PFC300은 복잡한 애플리케이션을 위해 설계된 강력한 컨트롤러로, 첨단 듀얼 코어, 64비트 프로세서와 2GB RAM을 탑재했습니다.
Popular PLC choices for large scale applications
Built for demanding industrial environments, these can deliver top performance, and scale for large implementations. These often have more advance motion and process control, along with high-speed communication, and large I/O counts. These are most suitable for Industry 4.0 and robotics applications.
Modicon M221 Programmable Logic Controllers
Schneider Electric’s Modicon M221 programmable logic controllers have a variety of certifications offering tremendous versatility.
Popular PLC content
12VDC PLC(Programmable Logic Controller, 프로그래머블 로직 컨트롤러)도 있나요?
대부분의 PLC는 24VDC의 공급 전원으로 동작하도록 설계되어 있습니다.
Communication Protocols
Comparison Table of Different Industrial Communication Protocols
Simple and widely used serial communication standard found in legacy industrial systems. Has limited transmission data rate (maximum of 115.2 kbits per second,) Modbus is popular because of its royalty free implantation and simplicity.
Modbus has two common variants:
- Modbus RTU (Remote Terminal Unit) - this is the most common version of Modbus and uses serial communication.
- Modbus TCP (also Modbus-TCP) - uses the Modbus RTU protocol with a TCP (Transmission Control Protocol) interface that runs on Ethernet.
PROFIBUS is short for Process Field Bus. It's a moderate data speed protocol for industrial automation. PROFIBUS uses a bus topology with controller devices and field sensors.
Despite the similar names PROFIBUS is not related to PROFINET. PROFIBUS is not based on ethernet and is generally an older protocol that is being phased out.
PROFIBUS has two variants:
- PROFIBUS DP (Decentralized Periphery) - is commonly used to communicate to industrial sensors and actuators and is commonly referred to as PROFIBUS (as this is the most frequently used variant.)
- PROFIBUS PA (Process Automation) – a variant tailored to operate in hazardous and explosive environments. In contrast to PROFIBUS DP, both data and power are transported over the same cabling.
PROFINET is short for Process Field Network. It's a scalable Industrial Ethernet protocol for collecting data and controling industrial equipment. It is based on ethernet, has support for real-time communication and deterministic data transfer, for synchronous control.
PROFIBUS and PROFINET are both IEC standards created by the same organization: PROFIBUS and PROFINET International (PI). Because of their common source, PROFIBUS and PROFINET do share some similarities. But they are very different with PROFIBUS being a serial-based communication and PROFINET being ethernet based.
CANopen is a higher layer CAN (Controller Area Network) based communication protocol for embedded device networks. It allows for off the shelf components and devices (from different manufacturers) to network together. CANopen was original designed for robotics and motion handling applications, but has also found widespread adoption in building automation, automotive, and medical devices as a common and easily implanted networking stack.
DeviceNet is an application layer protocol, that uses the CAN Bus physical and data link specifications along with the Communications and Information Protocol (CIP) which provides message information and object identification as an open standard supported by Open DeviceNet Vendors Association (ODVA.)
EtherCAT is an ethernet based fieldbus, for low latency and synchronization applications. Extremely fast, with synchronization times under 1 microsecond and deterministic real time communications. EtherCAT is ideal for motion control and high-performance automation, however the high hardware complexity and compatibility issues may be an issue for older hardware systems.
Source: Optimizing Industry 4.0 Communication Architectures using Multi-Protocol I/O Hubs and Converters
IO-Link is a short distance point to point digital communication standard used for Bi-directional communication with sensors and actuators. While IO-Link is not a field bus, the use of standard 24 VDC for power and unshielded M-12 connector 3 conductor cabling (as an agreed upon interface connector) makes IO-link an attractive alternative to many short run communication standards.
Popular junction boxes for communications
Weidmüller의 I/O 시스템 IP20 u-remote는 맞춤형 계획, 빠른 설치, 안전한 시동, 다운타임 최소화와 같은 사용자 이점에 중점을 둡니다.
Popular content for communications
EtherNet/IP와 PROFINET 비교
기업들이 디지털 방식으로 연결됨에 따라 산업 이더넷 채택이 계속적으로 다른 옵션을 앞지르고 있습니다. EtherNet/IP와 Profinet의 차이를 알아보세요.
2021 EtherCAT 업데이트
EtherCAT은 이더넷 데이터의 텔레그램 구조를 사용하여 1차 장치 및 1차 장치와 작업 현장의 2차 센서/액추에이터와의 관계를 설정합니다.
Programming languages for PLCs
The International Electrotechnical Commission (IEC) standard 61131 section 3 outlines the five different PLC programing languages most common for programming PLC, we'll discuss them below.
The 5 PLC programming languages standardized by IEC 61131-3 standard
Ladder Diagram (LD) / Relay Logic / Ladder Logic
Picture from PLC Programming Language Introduction
Ladder Diagram, also known as Ladder Logic or Relay logic is a widely used graphical programming language that mimics the original relay logic and wiring diagrams that were used in process control before PLC devices were developed. Great for simple on/off interfaces, logic control, and safety interlocks, LD is still favored in modern PLC programming as it easy to get started with and logically consistent with each rung of the ladder detailing the input and control devices as read from top to bottom and left to right.
Function Block Diagram (FBD)
Picture from User-Defined Function Block (UDFB) in Function Block Diagram (FBD) Using Siemens TIA Portal
Function Block Diagram (FBD) is graphical programming language for PLCs that describes the functional relationship between input and output variables of the control process.
Each block used in the graphical diagram are used to represent different logical operations or coding functions. The left to right connections and flow lines between these blocks show the path data takes flowing between these functions. FBD is great for process control and PID loops as the function blocks and looping paths closely match.
Sequential Function Chart (SFC)
Sequential Function Chart (SFC) is a graphical programming language used in PLCs useful for operations that have multiple states of operations or require state machine diagrams. SFC can look like a flowchart, with boxes representing steps (with actions required), transition functions (controlling the process flow between steps), and branch (if the process needs to operate in parallel sequence). SFC is great for modeling state machines, and machine sequences as the process can be modeled with logical control inputs and operations.
Structured Text (ST)
Structured Text (ST) is a text-based programming language for programming PLCs that more closely resembles common computer programing languages such as C++ or Pascal. Due to ST's syntax structure and list of high-level programming statements, the implementation of coding loops, logical value calculations, and data handling routines is easily accomplished which makes it a good starting point for PLC programmers that have background in more traditional computer programming.
Instruction List (IL)
Instruction List (IL) is a text-based programming language for PLCs. A low-level coding language (IL) can be though to resemble Assembly programming language, with direct operating statements and data control actions.
As of the third edition of the IEC 61131-3 standard released in 2012, IL was deprecated and not recommended for new projects. Still available and supported by some PLC hardware due to the long support time of industrial PLC hardware. It is becoming phased out and being replaced by other more flexible programming languages.
CODESYS
Software development environment that is IEC 61131-3 compliant. It's accepted by multiple different PLC manufacturers and therefore allows a developer to have a development environment that is not solely based on a single manufacturer.
Other Languages
As PLC processing power increases, more programming languages are becoming commonly used for PLC programming (including C++ and Python). These flexible, modern languages are acting as the intermediate layer between the PLC and other applications such as networking with PCs and other workstations. That said, there are drawbacks to consider for real time control applications (for example, redundancy and life cycle upkeep costs) when using a non-IEC 61131-3 language.
Popular Programming Content
PLC 프로그래밍: Siemens 예를 통한 기계 요약
4차 산업 혁명과 인더스트리 4.0에서는 고급 제어, 모니터링 및 진단에 의해 포괄적이고 지능적인 자동화가 정의됩니다.
복잡하고 중요한 자동화 프로세스의 배포 속도를 향상시키는 새로운 PLC
프로그래밍 가능한 새로운 논리 컨트롤러는 고급 기능과 복잡한 인프라와 자동화 프로세스를 빠르게 개발 및 배포할 수 있는 유연성을 결합합니다.
Movement and Actuators
Actuators are like the muscles of automation equipment. Actuators move the parts of the equipment (could be conveyor belts that spin or robotic arms that pick up objects).
Actuation power sources come in many different types as seen on the chart above
Motor Control / Electrical motors
Electrical motors are one of the simplest applications providing rotational power for Fans, pumps or conveyor belts.
Most motors require additional circuity and components such as motor drives for DC motors or Variable Frequency Drives (VFD) for controlling large AC motors
Solenoids / Relays / Contactors
Electromechanical devices that pass electrical current through a coil to provide movement.
A solenoid is made up of a coil of wire and the moveable plunger placed inside the coil also called an armature. When electrical current is applied to the end of the coil a magnetic field is generated that moves the armature, turning electrical energy into mechanical force. With a quick response time, compact size and simple operation, solenoids are a popular choice in industrial applications such as valve control for fluids and gases.
A relay is a device that uses low power electrical signals to control and switch higher electrical power circuits. A Relay is made up of a coil of wire generating a magnetic field and a separate switch circuit that closes an electrical circuit when the magnetic field is generated. Typically, relays can switch up to a few amps of current and a hundred of volts on the high-power side, but exact power ratings are dependent on the device and application. Relays simplicity and reliable design make them a popular choice for power switching for industrial and automotive applications.
A contactor is a device that uses low power electrical signals to control and switch much higher electrical power circuits. Unlike relays that switch a few amps of electrical current on the switching side of a Contactor. A contactor can switch dozens or hundreds of amps of electrical current and thousands of watts of electrical power. The robust design and internal components of most contactors make them preferred when switching high power electrical loads such as fans and motors.
Mechanical positioning devices, usually powered by a rotational motion source like an electrical motor which is mechanically converted to create linear motion. This includes
- Ball screw driven using ball bearings between the central shaft and nut used in applications needing a high level of accuracy and stability
- Lead screw driven for applications requiring a low-cost and simplicity
- Belt driven using a toothed belt to provide motion
Fluid power (Pneumatics / Hydraulics)
Some automation systems are powered by the movement of pressurized fluid (this could be gases like air or oil). These systems Pneumatic (air-driven) or Hydraulic (fluid-driven) are connected components that can be quickly installed and provide either linear or rotational power to devices.
Pneumatic (air-driven) systems typically operate under low pressure of 60 to 120 PSI powered by an air compressor and properly sized storage tank. Hydraulic (fluid-driven) systems operate at much higher pressures anywhere from 800 to 5000 PSI and have oil as a working fluid. Products include:
Indicators / Alarms
There are several devices that can be connected to automation systems to inform operators of system status and operating conditions. The simplest and most direct are indicator lights and audio alarms.
The classic tower lights can offer a color-coded status light informing staff on the floor of the machine operating status or if there are any error that need to be cleared. While some are simple indicator lights, other tower light devices are networked end terminals and can be remotely controlled or send messages across a network.
Audio devices such as buzzers, speakers or other sound generating can also be used for indicating machine status generating attention on a noisy shop floor.
What is the difference between a soft starter and a VFD ? View Answer
A Soft Starter and Variable Frequency Drive (VFD) are both types of motor starter devices, the design and use of both vary.
Both are semiconductor-based devices used to protect AC induction motors from the high inrush current (this occurs immediately during power on and slowly bring motors up to operational speed).
Most soft starters use a series of thyristors or silicon controlled rectifiers (SCRs) to reduce the inrush current. These get used in mechanical systems such as conveyer belts, or pumps.
A VFD can control the speed of the motor during the start and stop cycle, as well as throughout the run cycle. VFDs convert input power to adjustable frequency and voltage source for controlling speed of AC induction motors.
A soft starter is just focused on ramping up voltage and current.
Popular Actuator Content
전자 기계 액추에이터 대신 유압식 및 공압 액추에이터를 사용해야 하는 이유
유압식 및 공압 액추에이터는 반복적인 사용 메커니즘에서 전력과 속도를 제공합니다. 각 유형은 고유한 이점과 기능을 제공합니다.
솔레노이드 및 스테퍼 모터 구동기를 산업 응용 분야에 맞게 조정하는 방법
솔레노이드 및 스테퍼 모터 응용 분야의 개발자는 정교한 구동기 IC를 활용하여 성능을 개선하고 IoT 통합을 구현할 수 있습니다.
Robotics
The use of robotic ecosystems in industrial automation is steadily growing. In this rapidly growing space, DigiKey has a wide range of robotic systems and components in stock and available for next-day delivery.
For more information about robotic platforms and applications, please visit our Application and Technology page on Robotics.
Also, relevant robotics topics are covered within the DigiKey eMagazines on Robotics.
Industrial Sensors
Industrial sensors are the eyes and ears for PLCs. These sensors, monitor and analyze incoming signals to provide the first step of the feed back loop in process monitoring. These measurements include temperature, pressure, and proximity distances.
Pressure
Pressure sensors can measure the amount of pressure (of gases or liquids). This is usually done to maintain safe and efficient operation within a system. There are a few different types of pressure sensors depending on measuring method being used. Some of the most common include:
- Gauge - relative to current local atmospheric pressure
- Absolute – Measures pressure relative to a perfect vacuum
- Differential – measured the pressure difference between two pressure points, typically between two vessels
Photoelectric
Photoelectric sensors can determine the presence of an object (or measure a distance) by measuring the changes in the transmitted light beam. When the beam of light has been interrupted or blocked from the receiving sensor an object can be inferred, and action can be taken.
Time of flight and distance sensors are similar although they project and receive the light beam back. By measuring the time it takes for a light beam to be reflected off an object a distance measurement can be determined.
Proximity
Proximity sensors can detect presence and distances to objects without physically touching them. Useful for object detection safety interlocks and verifying objects are present (for quality control).
Here are some common methods that proximity sensors operate based on:
- Inductive - by detecting changes in rapidly changing electromagnetic field project outward from the sensor, an inductive sensor can detect the present of a ferrous (iron) and non-ferrous (non-iron based) metal objects.
- Capacitive - as a metallic and non-metallic object approaches the capacitive sensor it disrupts the electrostatic field by changing.
- Magnetic - the presence of a magnetic field approaching the sensor face can be detected by the changes in output by Giant magneto resistive (GMR) sensors or resonant circuits, useful for detecting when a known object is approaching like a safety door or tool head.
Temperature
Sample Image Text
Temperature sensors measure thermal conditions and local temperature in process for control and monitoring and to avoid overheating and thermal runaway conditions. Temperature sensors can either be contact and changing electrical properties or by measuring the infrared energy given off.
Distance
Sample Image Text
Determining the distance from a sensor to an object (either stationary or moving) is of great importance to the modern factory. AMRs and other robotic platforms can navigate and make sure the work area is clear of any obstructions.
- Ultrasonics: A transmitter emits a short burst of high-frequency sound waves. When this pulse of sound hits an object, some of the sound waves are reflected to the receiver. A common application for ultrasonic sensors is contactless liquid and fluid level measurement within a tank.
- Radar: Like ultrasonics, radar sensors send out short bursts of high-frequency energy and measure distance based on the time it takes for the reflection to bounce off the surface. Instead of sound waves, radar uses microwave radio waves.
- Lidar: By rapidly spinning a light source like a laser and calculating the time it takes for the light to return to the receiver Distance from the LiDar sensor can be found. Much like Radar it allows for high accuracy.
Rotational
The speed of a rotating shaft or position of the slider can be measured by an encoder, which is an electro-mechanical device that converts the position or motion of a shaft or axle to analog or digital output signals.
Force and Load Cells
Load cells convert forces (like weight, compression, tension, or torque) into measurable signals. As the force applied changes, the output signal changes proportionally. Load cells are commonly used in industrial applications to control weight capacity, measure products, or track weight changes over time.
Popular Industrial Sensor Products
Popular Industrial Sensor Content
로보틱스 및 산업 응용 분야를 위한 정밀 공압 압력 모니터링
정밀 압력 모니터 및 이러한 정밀 압력 모니터가 산업 및 로보틱스 응용 분야에서 공압 및 압축 공기 시스템의 요구 사항을 충족하는 방법에 대해 논의합니다.
온도 컨트롤러와 Micro PLC를 사용하여 소규모 자동화 프로젝트 가속
중소형 기계에 최적화된 온도 센서 기술 및 PLC와 관련된 문제를 살펴보고 전력 및 히터 컨트롤러를 검토합니다.
Safety
Disclaimer: The following information is for educational use only and does not represent safety consulting or design verification. Please consult with a qualified safety technician or inspector before working on any equipment and always be sure to read and follow any safety instructions that come with your industrial equipment.
There are many dangers in the modern industrial process from overheating and runaway pressure to energized machines and faulty sensors. It takes a well-designed system with strict standards to keep both the operators and machine protected.
Regulatory Agencies
-
Occupational Safety and Health Administration (OSHA) - United States government agency within the US Department of Labor sets workplace safety regulations designed to protect worker and prevent workplace accidents
- Underwriter Labs (UL) – global organization that tests and certifies electronic products for quality and safety.
- National Electrical Manufacturers Association (NEMA) – association electrical equipment that publishes safety standards.
- The International Electrotechnical Commission (IEC) - is an international standards organization that prepares and publishes international standards for all electrical, electronic, and related technologies.
Safety Integrity Level (SIL)
The Safety Integrity Level (SIL) is a functional safety term for the level of risk reduction provided by safety equipment. Based on the IEC 61508 standard there are four levels of SIL with level 1 being the least dependable and level 4 being the most dependable level of safety.
For PLCs this can mean detecting faults, executing safe state, and maintaining the certified operation.
Performance Level (PL)
Performance level (PL) is used to define the likelihood of products to perform safely (thus avoiding dangerous failures). PLe is the lowest likelihood of dangerous failure (0.000001% to 0.00001% probability).
Products
Safety light curtains are optoelectronic devices used to protect personnel from hazardous machinery. They create an invisible barrier of infrared beams between a transmitter and a receiver pair of devices. When any beam is interrupted, the system sends a signal to stop the machine immediately.
Operator presence mats are pressure-sensitive safety devices placed on the floor near hazardous machinery. When stepped on, they detect the presence of a person and trigger a control signal, typically to stop or prevent machine operation.
Safety interlocks are mechanical or electrical, based devices that prevent machinery from operating under unsafe conditions. They are typically installed on movable guards, doors, or access panels to prevent operations when open or misaligned and are integrated into a machine's control system.
Emergency stop switches (often called E-Stops) are manually operated safety devices and mechanical switches that are designed to immediately halt machinery or equipment in the event of a hazard.
Lockout devices are physical safety tools used to isolate switches and prevent the accidental startup of machinery or equipment during maintenance, cleaning, or repair. They are a core part of Lockout/Tagout (LOTO) procedures, which are mandated by OSHA under standard 29 CFR 1910.147.
Laser scanners are non-contact protective devices that use laser beams to monitor defined zones. If a person or object enters a protected area, the scanner sends a signal to stop nearby machinery, preventing injury or damage.
Popular Safety Devices
Popular Safety Content
안전 인터록의 기본 사항
공장 작업자를 안전하게 유지하기 위해서는 기계적 위협으로 인한 신체적 위해로부터의 보호가 필요합니다. 이 분야를 산업 위험성 축소 분야하고 합니다.
적절한 안전 컨트롤러 선택의 복잡성 해결
산업 시스템의 안전은 매우 중요하고 복잡한 주제이므로 주어진 응용 분야에 가장 적합한 안전 컨트롤러를 지정하는 데 어려움이 있습니다.
안전 등급 접촉기를 사용하여 최적의 산업 안전 솔루션을 실현하는 방법
고장 시 안전 작동 기능을 갖춘 Siemens의 3RT2 안전 등급 접촉기를 사용하여 최적의 산업 안전 솔루션을 실현하도록 안전 시스템을 설계하는 방법을 소개합니다.
Machine Vision
Machine vision devices enable systems to rapidly view products moving along a conveyor and make real time decisions (often within fractions of a second) such as identifying defects or determining where a product should be diverted. This capability is driven by machine vision software, with models tuned for specific applications including pattern matching, optical character recognition (OCR), barcode decoding, and color analysis.
Barcode readers and Machine Vision systems may seem similar but have different applications
Barcode Readers
Barcode readers can quickly and efficiently read barcode labels. This could be a 1-dimensional barcode or 2-dimensional square barcode. Due to focused nature of only reading barcode labels these systems are typically easy to implement and have high throughput rates but are unable to do anything but read clear barcode labels. The use of standardized data and consistent label locations makes barcode systems perfect for tracking items and logistics where items passing by a fixed scan location can be read.
Machine Vision Cameras
Machine vision cameras are great at analyzing characteristics of an object and are often used for defect management and quality control of products. By comparing known good images from the training set to the incoming data from cameras, items can be identified as good or defective with minimum human involvement. Machine vision cameras can be used for multiple tasks (including reading barcodes) though operators need to balance resolution and framerates to manage overall bandwidth limitations of the system.
2D vs 3D Vision
2D and 3D Machine Vision systems have different strengths and weakness
Machine vision can either be 2D or 3D depending on the set up. While there is no single option that is better than the other there are differences between the two:
- 2D is good for understanding surfaces. This can include presence sensing and measurement. 2D vision systems are often used in environments that have more clearly defined distances the objects will be recorded at.
- 3D is good for understanding volumes. This can include sensing depth or measuring the distance to an object. 3D vision systems are typically found in more dynamic environments where objects or pathing could change and accurate measurements are needed.
Popular Machine Vision Products
Advantech의 iCAM-520 계열 산업용 AI 카메라에는 NVIDIA Jetson Xavier NX 컴퓨팅 모듈이 장착되어 있으며 개발 키트로도 제공됩니다.
Popular Machine Vision Content
산업용 시스템에 머신 비전을 빠르게 추가하여 공장 안전성 및 생산성 향상
객체 깊이 감지 기능이 있는 머신 비전을 산업용 시스템에 손쉽게 추가하여 안전성, 생산성, 효율성을 향상시킬 수 있습니다.
즉시 생산 가능한 플랫폼으로 적응형 에지 비전 응용 제품을 빠르게 제작하여 배포하는 방법
비전 중심 하드웨어와 소프트웨어는 적응형 스마트 비전 응용 분야의 개발을 간소화합니다.
스마트 머신 비전 시스템을 빠르게 설계하고 배치하는 방법
머신 비전은 보안, 교통 카메라, 자동 검사, 공정 관리, 비전 가이드 로봇을 비롯한 여러 응용 분야에서 성장하고 있습니다.
사용하기 쉬운 카메라 모듈로 응용 제품에 간편하게 머신 비전 추가하기
완벽하게 구성된 카메라 모듈과 사용하기 쉬운 소프트웨어를 활용하여 머신 비전을 위한 렌즈 및 광학 구성을 빠르게 평가하세요.
Conveyor Block Diagram
Circuit Protection and Line Filter
Eaton Power Defense™ 몰드 케이스 회로 차단기는 글로벌 등급으로, 설치 공간이 작아 여러 응용 제품에 쉽게 적용할 수 있습니다.
Uninterruptible Power Supply (UPS)
Tripp Lite by Eaton의 DIN 레일 UPS는 열악한 환경에 적합하며, 스마트하고 연결된 산업용 응용 제품을 위한 안정적이고 유연한 전력 보호 기능을 제공합니다.
DUSH960 DIN 레일 마운트 DC 무정전 전원 공급 장치
TDK-Lambda의 DUSH960 DIN 레일 마운트 DC 무정전 전원 공급 장치(DC-UPS)는 정전 시 백업 전원을 공급하기 위해 두 가지 기능을 수행합니다.
SMPS 24 VDC
MEAN WELL XDR-E 및 XTR 계열 DIN 레일 토탈 솔루션은 산업용 전력 시스템을 간소화하고 최적화하도록 설계되었습니다.
Phoenix Contact의 TRIO IP67 전원 공급 장치는 제어 캐비닛의 제한을 없애고 사용자가 전원이 공급되는 기계에 장치를 직접 배치할 수 있도록 합니다.
Hold up / Buffer
PLC
For more detailed product listing of PLC by application size, please see the first section of page.
IO Modules and Relays
Phoenix Contact의 Axioline XC 및 EX I/O 모듈은 Class I, Div 2 환경에 설치하도록 설계되었으며 엄격한 UL-Ex 승인 테스트를 거쳤습니다.
Motor Control
TeSys™ D 접촉기, Altivar™ 공정 구동기, 혁신적인 Harmony™ 푸시 버튼과 같은 Schneider Electric의 포괄적인 모터 제어 솔루션을 살펴보세요. 이러한 솔루션은 정밀 모터 제어, 고급 보호 기능 및 완벽한 통합을 제공합니다.
Communications Block
Weidmüller Basic Line 시리즈 B는 PROFINET CC-A 및 이더넷/IP 네트워크를 지원하는 관리형 스위치에 대한 비용 효율적인 대안을 제공합니다.
OPC UA 및 MQTT 인터페이스를 갖춘 IO-Link 마스터
Pepperl+Fuchs IO-Link 마스터 계열은 업계 최고의 프로토콜을 지원하고 OPC UA 및 MQTT 인터페이스와 실시간 필드버스 프로토콜을 제공합니다.
Motor
Sanyo Denki SanMotion Products의 서보 모터는 높은 서보 성능과 신뢰성을 제공하여 다양한 지역과 환경에서 사용자에게 마음의 평화를 제공합니다.
Schneider Electric의 Lexium 32 서보 구동기 제품군에는 LXM32C, LXM32A, LXM32M, LXM32S의 4가지 서보 구동기 모델이 포함되며, 두 가지 서보 모터 제품군과 결합됩니다.
Cameras and Sensors
Delta의 산업용 카메라는 이더넷 연결과 함께 GigE Vision® 및 GenICam 표준을 갖추고 있어 높은 호환성, 안정성 및 유연성을 제공합니다.
Orbbec의 Gemini 435Le 산업용 스테레오 비전 카메라는 물체의 가장자리와 윤곽을 우수하게 재현하는 기능을 제공합니다.
Sourced from:
Picture from
Picture from
Block Diagram of a Conveyor System