Slide 1
Slide 2
Slide 3
Slide 4
Slide 5
Slide 6
Slide 7
Slide 8
Slide 9
Slide 10
Slide 11
Slide 12
Slide 13
Slide 14
Slide 15
Slide 16
Slide 17
Slide 18
Slide 19
Slide 20
Slide 21
Slide 22
Product List
This type of power circuit is known as a Distributed Power Architecture (DPA) and they are commonly used in circuit power designs. The DPA is characterized by driving a single bus voltage to feed multiple POL converters. It has also brought with it the benefits of lower cost, weight, and space along with a better quality of power. In stage 1 of power conversion, an AC-DC power supply is used to convert a line voltage to a DC bus voltage of 48 V, 24 V, or 12 V. If 48 or 24 V is used to feed the circuit, the power rail is then converted to 12 V or 5 V through an isolated DC-DC converter; this is called stage 2 conversion. As a side note, if 12 V is fed directly to the circuit load as shown on the right side of the circuit pack here, the isolated conversion used in stage 2 is not required. Conversion can proceed directly to stage 3. Stage 3, the final conversion stage, is used to reduce the 12 V or 5 V bus to the various voltages required to drive the individual semiconductor loads, like an FPGA, CPU, or DSP.
PTM Published on: 2015-06-18