기사 및 블로그

DigiKey Marketplace 및 Fulfillment 서비스 게시 날짜: 2021-03-30

DigiKey는 최근 새로운 시장으로의 공격적인 확장에 도움이 되는 두 가지 프로그램을 선보임으로써 많은 공급업체 또는 유통업체에 새로운 기회를 제공하고 있습니다.

Digi-Key IoT 셀룰러 데이터 플랜

Digi-Key에서 RevX를 통해 제공되는 새로운 셀룰러 데이터 플랜 발표! 이 플랜은 IoT 장치를 지원하는 빠르고 간단한 방법을 제공합니다.

Basics of Oscillators

Timing is critical in nearly every electronic application in the world. Oscillators control timing in microprocessors, MCUs, SoCs, and many other things.

SmartBond DA14586 BLE SoC

The Dialog Semiconductor DA14586 is a Bluetooth Low Energy device that has some great development tools including an evaluation board.

Oscillator Tutorial 게시 날짜: 2017-11-09

An examination of some of the main types of oscillators, some of the typical terms used in the industry, and how to find oscillators on the DigiKey website.

Basics of Circuit Breakers

No matter how good a design is, it can still be subject to events out of the engineer’s control. Circuit breakers can help protect against these events.

Module or Discrete Power Blog

A discussion of some of the advantages of using power modules over discrete power, highlighting the VMS-365 series and the PBO-5 series from CUI.

AS3935 Lightning Sensor

The AMS AS3935 lightning sensor is designed to help users detect lightning from up to 40 km away.

Circuit Breakers 게시 날짜: 2017-10-17

There are many circuit breaker options. This article provides guidance on the different types of breakers available, their differences, and mounting choices.

The ASX10108-SPD-R Audio Exciter

The ASX10108-SPD-R exciter from PUI is an 8 Ω exciter which works similar to a traditional loudspeaker but uses whatever surface it is set on to produce sound.

Basics of Fuses

A fuse is a device that is intended to protect a piece of electronic equipment. They are inexpensive compared to the equipment they are protecting.

Fuse Tutorial 게시 날짜: 2017-10-03

A discussion of the different considerations for choosing a fuse, some of the industry vernacular, and applications for different kinds of fuses.

Basics of Switches

Pat discusses the basics of switches and outlines his recently written "Switch Tutorial" article.

스위치 튜토리얼 게시 날짜: 2017-09-21

거의 모든 전자 장치에는 스위치가 최소한 하나 또는 여러 개 있습니다. 이 기사에서는 스위치와 스위치의 일반적인 응용 분야에 대해 설명합니다.

Basics of ADC/DAC

This blog highlights the “ADC/DAC Tutorial” article posted on the DigiKey website. This article covered ADC/DAC architectures along with their key parameters.

Murata DC-DC Converter

A brief discussion of the LXDC2HL18A-052, a low power DC step-down converter, from Murata. This device has an output of 1.8 V and of 600 mA.

ADC/DAC 자습서 게시 날짜: 2017-09-13

아날로그 디지털(ADC) 신호 변환 또는 디지털 아날로그 신호 변환(DAC)은 불가피한 작업입니다. 이 기사에서는 다양한 종류의 ADC 및 DAC에 대해 설명합니다.

Basics of Connectors

There are thousands of different connectors on the electronics market. This is a basic overview of the connector types found on digikey.com.

Connector Tutorial 게시 날짜: 2017-09-05

There are many different kinds of connectors, all serve the same purpose but in different ways. This article discusses connectors and their typical applications.

Initial State

Initial State’s analytics service streams data onto the Initial State dashboard to enable monitoring of devices and events from a browser.