Basics of Oscillators

Timing is critical in nearly every electronic application in the world. Oscillators are used in various applications including controlling the timing in microprocessors, MCUs, SoCs, and many other things. Different applications call for different types of oscillators. Often there are concerns that can be addressed by a certain type of oscillator. Factors such as physical size, environmental requirements, and necessary output need to be taken into consideration. I recently wrote an article titled “Oscillator Tutorial” that briefly touched upon the differences between some of the different kinds of oscillators in the market today and how to find these products on the DigiKey website.

Crystal oscillator (X0)

  • One of the most popular oscillators
  • Uses a crystal element to determine output frequency
  • Has a fixed frequency output

MEMS oscillator

  • Uses etched silicon in a die acting like a tuning fork at a resonant frequency
  • Uses silicon technology which is less expensive to manufacture than quartz crystal
  • Consume less current than a crystal oscillator

Voltage Controlled oscillator (VCXO)

  • Ability to change frequency based on input voltage
  • Has a specified range of frequency over a specified voltage range
  • Useful in Phase Lock Loop applications

Temperature Compensated oscillator (TCXO)

  • Made to compensate for temperature changes
  • Uses compensation network to do this
  • Typically incorporates a thermistor and a varactor

작성자 정보

Image of Pat Sagsveen DigiKey의 응용 프로그램 엔지니어링 기술을 담당하고 있는 Pat Sagsveen은 고객이 프로젝트를 완료하는 데 새로운 기술과 부품을 활용할 수 있는 보다 나은 방법을 찾도록 지원합니다. Pat은 비스마르크 주립 대학에서 전자 및 통신 응용과학 준학사 학위를 취득한 후 2016년에 DigiKey에 합류했습니다. 증폭기 매니아인 Pat은 여가 시간에 3 진공관 기타 증폭기 등을 증폭기 제작을 즐깁니다.
More posts by Pat Sagsveen
 TechForum

Have questions or comments? Continue the conversation on TechForum, Digi-Key's online community and technical resource.

Visit TechForum