New Product Discoveries - PUI Audio's Exciter and Pimoroni's micro:bit Development Board

Today on New Product Discoveries I have an Exciter from PUI Audio and the micro:bit educational development board from Pimoroni.

PUI Audio has traditionally been known for their speaker products. Today, we are presenting a product called an Exciter (ASX08808-TP-R). Similar to a speaker, an Exciter is a voice coil that is made to be mounted on a hard surface. The inherent dynamic quality of the surface in which the Exciter is mounted is what affects the emitted frequency color. The advantage of an Exciter over a traditional speaker is that sound is emitted in a planar fashion. This means the emitted sound waves are more easily picked up without having to be directly in front of the Exciter.

Another product I would like to discuss is the micro:bit educational board from Pimoroni. Pimoroni is well known for their offering of educational tools and kits – the micro:bit is no different. The micro:bit prototyping kit comes with all the required accessories to get you creating micro:bit projects with ease. The micro:bit is programmed through a graphical form which lends itself to teaching children microprocessor programming. There are a few different micro:bit kits available, and the board alone can be purchased as well – all on digikey.com.

Thank you for listening!

작성자 정보

Image of Randy Restle

Randall Restle은 전자 부품 업계에서 40년 넘게 경력을 쌓아왔습니다. 현재 현직에서는 은퇴했으며, DigiKey에서 응용 분야 엔지니어링 부문 부사장을 역임했습니다. 숙련된 응용 분야 엔지니어, 기술자 및 관리 인력으로 구성된 팀을 이끌며 독창적이고 고유한 고급 기술 제품을 개발하도록 하는 등의 직무를 수행했습니다.

개인적으로 관심 있는 분야로는 디지털 신호 처리, 프로그래밍 가능한 로직 구현, 동작 제어 개선 및 소프트웨어 설계 등이 있습니다. 다양한 업계에 걸쳐 특허를 보유하고 있으며, IEEE의 수석 회원입니다. Randall은 신시내티 대학에서 BSEE, MS, MBA 학위를 취득했습니다.

More posts by Randall Restle
 TechForum

Have questions or comments? Continue the conversation on TechForum, Digi-Key's online community and technical resource.

Visit TechForum