The WiFi Continuum

작성자: Steve Leibson

Electronic Products 제공


On his blog, "The WiFi Decade," Dana Blankenhorn recently commented on how we have all become accustomed to the pervasiveness of WiFi in everyday life. He starts out by commenting that he is working in the reference room of the San Antonio public library, which provides free WiFi. He continues by noting that WiFi hotspots are becoming increasingly common in public spaces, particularly coffee shops, and that the WiFi bandwidth is free in a growing number of cases.

"Paid WiFi is going the way of the dodo," writes Blankenhorn. If true, this situation is quite different from even a few years ago when the installation of WiFi hotspots and the creation of countrywide, for-pay WiFi networks was viewed as an up and coming business model. Now, the store offering a WiFi connection is likely piggybacking on its own all-you-can-eat Internet connection, used primarily for its own business. Adding WiFi for customers is often a matter of adding one or two $40 access points, and away you go. Add in the coming of the automotive hotspot and the growing availability of hotspots on aircraft, and you quickly start to see a world where WiFi access is pervasive and ubiquitous.

What does this mean to you, the embedded designer? It means that you might, under certain circumstances, start to rely on the pervasive ability of WiFi access in a way resembling the ubiquitous availability of cellular telephony networks. Although standards such as WiMAX are exciting to contemplate, maybe WiFi is all you need. In fact, WiFi access points are becoming so ubiquitous that you often have access to two, three, six, or a dozen WiFi access points from any given location. That’s a log of free, global connectivity. It’s sort of hard to ignore, isn't it?

Blankenhorn's blog really makes you think. There is quite a bit of merit to this concept. WiFi is a well-developed standard. Designers have been extending WiFi’s use for unplanned applications for years and continue to do so. The hardware is well in hand – it is installed in tens of millions of laptops, desktop PCs, and wireless access points each year. WiFi has been wrung out, ironed out, and taken to the point where you might very well consider using it for diverse embedded applications.

You can add WiFi to your embedded design through a variety of means, from simple to complex. One of the simplest, called serial-to-WiFi by Digi International, converts a simple asynchronous serial port to a WiFi connection in the way that serial-to-Ethernet converters have connected simple embedded systems to Ethernet networks for years. If your embedded system needs to talk to just one client or server on the network, the simple approach may be the one for you.

Does your application require more complex networking capabilities? If so, you need to add WiFi as a native networking interface, which provides full socket-level access, so you can run concurrent servers and clients. However, if you take this route, your design will suddenly need to understand all of the complex ins and outs of networking – it will need a full network stack. If you choose to go this route, you can select from a range of WiFi modules that connect over serial ports, processor buses, USB, and Ethernet ports. The one you select will probably depend on the design and the available ports on your existing embedded design.

면책 조항: 이 웹 사이트에서 여러 작성자 및/또는 포럼 참가자가 명시한 의견, 생각 및 견해는 DigiKey의 의견, 생각 및 견해 또는 DigiKey의 공식 정책과 관련이 없습니다.

작성자 정보

Image of Steve Leibson

Steve Leibson

Steve Leibson은 HP와 Cadnetix에서 시스템 엔지니어로 근무한 후, EDN 및 Microprocessor Report에서 편집장을 역임했습니다. 또한 "The Next Wave with Leonard Nimoy”에 기술 전문가로서 2회 출연한 바 있습니다. 그는 33년 동안 설계 엔지니어가 보다 빠르고 효율적이며 신뢰성이 뛰어난 시스템을 개발할 수 있도록 지원해 왔습니다.

게시자 정보

Electronic Products

Electronic Products 잡지와 ElectronicProducts.com은 전자 장비와 시스템 설계를 담당하는 엔지니어와 엔지니어링 관리자를 대상으로 합니다.