기사 및 블로그

Image of Measuring the Speed of Sound Using an Ultrasonic Sensor and Oscilloscope Measuring the Speed of Sound Using an Ultrasonic Sensor and Oscilloscope

In this blog, I will walk through a simple experiment that uses an ultrasonic sensor and oscilloscope to measure how fast sound travels through the air.

Image of Single-Chip Systems, MCUs for Matter-Enabled Smart Home Devices Fill Multiple Mesh Network Roles Single-Chip Systems, MCUs for Matter-Enabled Smart Home Devices Fill Multiple Mesh Network Roles 게시 날짜: 2026-03-31

Energy-efficient, low-latency components from NXP support Matter-enabled smart home networks while development tools help designers create new prototypes.

Image of Power Distribution Boards: Smart Alternative to Relays Power Distribution Boards: Smart Alternative to Relays

This blog will talk about the core concepts and the theory behind the circuit schematic and how it was approached.

Image of Harnessing AI at the Edge with iWave’s Agilex™ 5 System on Module Harnessing AI at the Edge with iWave’s Agilex™ 5 System on Module

As data processing increasingly moves closer to the edge, platforms that deliver efficient AI performance with low latency and high customization are needed.

Image of Webinar – Seven Reasons to Move from 12 V to 48 V Today 웨비나 - 지금 바로 12V에서 48V로 전환해야 하는 7가지 이유

48V가 대세 전력 공급 네트워크가 되는 이유, 그리고 모듈식 전력 솔루션으로 48V로의 전환을 가속화하고 간소화하는 방법을 살펴봅니다.

Image of Simplifying Frequency Stability for High-Speed 5G and Data Converter Designs 고속 5G 및 데이터 컨버터 설계에서 주파수 안정성 간소화하기 게시 날짜: 2026-03-25

VCO가 통합된 ADI의 ADF4382 PLL이 고속 데이터 컨버터 및 5G 무선 설계에서 주파수 안정성과 속도를 개선하는 방법을 알아보세요.

Image of Building Quantum-Resilient Embedded Systems with iWave’s Agilex™ 5 System on Module Building Quantum-Resilient Embedded Systems with iWave’s Agilex™ 5 System on Module

iWave Global has partnered with Xiphera to deliver quantum-safe cryptographic capability on iWave’s Agilex™ 5 System on Module (SoM) powered by Altera.

Image of How to Select Cables for Reliable VFD Motor Control and Sensor Feedback 신뢰할 수 있는 VFD 모터 제어 및 센서 피드백을 위한 케이블을 선택하는 방법 게시 날짜: 2026-03-24

산업 자동화의 성장과 에너지 효율 향상에 대한 요구로 인해 모터 구동 시스템에서 VFD 채택이 가속화되고 있습니다.

Image of Solder Smarter Using DigiKey Standard Helping Hands Solder Smarter Using DigiKey Standard Helping Hands

Explore DigiKey Helping Hands features including magnetic PCB pillars, flexible arms, LED magnifier, and a heavy steel base for stable soldering.

Image of Automotive Ethernet: The Backbone of Modern In-Vehicle Communication 차량용 이더넷: 최신 차량 내 통신의 핵심 기술

차량이 점점 더 자율화되고 데이터 중심화되면서, 고속, 확장성, 안정성을 갖춘 차량 내 통신 근간에 대한 필요성이 그 어느 때보다 커지고 있습니다.

Image of Webinar – Select the Right Cables for Harsh Industrial Automation Applications 웨비나 - 열악한 산업 자동화 응용 분야에 적합한 케이블 선택

이 심층 웨비나에서는 산업 환경에 적합한 전선 및 케이블을 선택하는 데 필요한 사항을 자세히 설명합니다.

Image of Pushing the Limits: A 6km LoRa Range Test with the PTSolns SX1276 Shield Pushing the Limits: A 6km LoRa Range Test with the PTSolns SX1276 Shield

In this blog, we’ll explore the hardware that’s being used, the science behind the transmission, and just how impressive a feat it is to achieve a 6km range.

Image of How Hardware Gets Hacked (Part 2): On-boarding How Hardware Gets Hacked (Part 2): On-boarding

Explore a hardware security workflow using firmware builds, simulation tools, serial commands, and automated tests for microcontroller systems.

Image of Detecting High-Impedance Ground Faults: Limitations of Standard GFDI and Active Diagnostic Solutions 고임피던스 접지 결함 감지 : 표준 GFDI의 한계 및 능동형 진단 솔루션 게시 날짜: 2026-03-18

표준 GFDI의 한계, 고임피던스 결함의 물리학, 1500V 어레이에서 이러한 결함을 찾을 때 마주하는 실질적인 과제를 살펴봅니다.

Image of Criteria for Cable and Wire Selection 케이블 및 전선 선택 기준 게시 날짜: 2026-03-17

케이블 설계는 시스템적인 사고와 함께 설치 방법, 전기 및 기계적 부하, 비용 효율성을 통합하는 데 중점을 두어야 합니다.

Image of Why We Need New Op Amps Despite Already Having So Many Good Ones 이미 양호한 연산 증폭기가 많은데도 새로운 연산 증폭기가 필요한 이유

구형 연산 증폭기는 설계자에게 신뢰를 주는 반면, 새로운 연산 증폭기는 자재 명세서(BOM)의 측면에서 공급업체에게 이익이 될 가능성이 높습니다.

Image of How to Overcome Linux Development Hurdles in Resource-Constrained Systems 리소스 제한적 시스템의 Linux 개발 장애를 극복하는 방법 게시 날짜: 2026-03-12

BeagleBoard.org BeagleV-Fire 단일 기판 컴퓨터가 리소스 제약이 있는 시스템에서 Linux 실행 시 일반적으로 발생하는 장애물을 해결하는 방법을 알아보세요.

Image of Webinar – Single Pair Ethernet — Simplified Sensor-to-Cloud Networking 웨비나 - 단일 쌍 이더넷 - 간소화된 센서-클라우드 네트워킹

단일 쌍 이더넷(SPE)은 산업용 연결의 판도를 바꾸었습니다. 이제 SPE는 데이터 라인을 통한 전력 공급 기술(PoDL)을 통해 데이터와 전력을 모두 제공할 수 있습니다.

Image of XRP CoreXY Chessboard Reimagined XRP CoreXY Chessboard Reimagined

Discover how the XRP CoreXY chessboard prototype evolved with improved durability, lighting effects, and a compact transportable design.

Image of How to Meet High-Speed Interface Requirements Using Hyper Cool Edge Connectors Hyper Cool Edge 커넥터를 사용하여 고속 인터페이스 요구 사항을 충족하는 방법

Hyper Cool Edge 커넥터 제품군을 사용하여 스토리지 및 AI 데이터센터와 같은 응용 분야에서 고속 데이터 인터페이스를 지원하는 방법을 알아보세요.