Maker.io main logo

What's the Difference Between the ZED-F9P and the ZED-X20P?

105

2026-02-24 | By SparkFun Electronics

Wireless GPS Other RF Qwiic

Courtesy of SparkFun

Guide by [redacted]

Introduction

The ZED-X20P is u-blox's GNSS receiver designed as a successor to the wildly popular ZED-X9P. It has improvements in accuracy, band reception, and power consumption. Here, we outline the key differences between our ZED-F9P and ZED-X20P breakout boards so you know exactly how to upgrade your projects to the newest technology.

Comparison of Features

u-blox provides the following table comparing key high-level differences between the features on the ZED-F9P and the ZED-X20P:

Image of What's the Difference Between the ZED-F9P and the ZED-X20P

We've also compiled the differences between the chips across more specific features:

Image of What's the Difference Between the ZED-F9P and the ZED-X20P

Notes: u-blox has recently removed support for the GLONASS GNSS constellation. This is not accounted for in the listed current consumption of the ZED-X20P.

Hardware Changes

With the exclusions of the added JST connector and adjusted location of the BlueSMiRF header; the overall board dimensions, edge connectors and screw-hole locations, and PTH pin layout are exactly the same.

Allband GNSS RTK Breakout - ZED-X20P (Qwiic)

Image of What's the Difference Between the ZED-F9P and the ZED-X20P

GPS-RTK-SMA Breakout - ZED-F9P (Qwiic)

Image of What's the Difference Between the ZED-F9P and the ZED-X20P

GPS-RTK2 Board - ZED-F9P (Qwiic)

Image of What's the Difference Between the ZED-F9P and the ZED-X20P

Antenna Connection

Connector Options

With the ZED-F9P we released two different boards with either a U.FL connector or an SMA connector to attach a GNSS antenna. With the ZED-X20P, we have released a single board with both options with a jumper to select the connector to be used.

SMA: The location of the SMA connector remains the same.

Image of What's the Difference Between the ZED-F9P and the ZED-X20P

U.FL: The U.FL connector’s location is slightly different by a couple millimeters. There was a hole in the board to pass a U.FL cable through.

Image of What's the Difference Between the ZED-F9P and the ZED-X20P

Notes: We did our best to maintain an impedance match between the two different connections. Users may experience a small shift in the signal’s impedance after altering their board. However, in our experience, the GNSS receiver was still functional after modifying the jumper and we didn’t really notice a degradation in performance.

Length of SMA Connector

We recently changed suppliers for our SMA connector, so users will eventually see a slightly longer SMA connector on future boards.

Image of What's the Difference Between the ZED-F9P and the ZED-X20P Old version: 6.3mm

Image of What's the Difference Between the ZED-F9P and the ZED-X20P New version: 8mm

BlueSMiRF Header Location

On the ZED-F9P boards, the BlueSMiRF PTH pins were located at the edge of the board. For the ZED-X20P, we have added a locking JST connector, in its place, to allow users to easily attach an RF transceiver. Therefore, the BlueSMiRF header was relocated to the interior of the board.

Image of What's the Difference Between the ZED-F9P and the ZED-X20P

Notes: The pin layout of the BlueSMiRF header remains the same; connecting to the UART2 interface of the GNSS receiver. On the ZED-X20P, we added a VSEL jumper for users to switch between either a 5V or 3.3V input/output voltage for the BlueSMiRF header.

Pin Functionality

Most of the pin functionality remains the same, with the exception of a single pin. The safeboot pin on the ZED-Z20P board was relocated to a test point and replaced with the enable pin for the RT9080 LDO.

Image of What's the Difference Between the ZED-F9P and the ZED-X20P ZED-F9P: Safeboot Pin

Image of What's the Difference Between the ZED-F9P and the ZED-X20P ZED-X20P: RT9080 Enable Pin

Notes: The SPI interface is enabled with the DSEL jumper for the ZED-F9P; meanwhile, for the ZED-X20P, it is enabled with the SPI jumper. The operation of these jumpers remains the same; only the name changed on the silkscreen. Similarly, the EVENT and INT pins are both external interrupt pins; only the name changed on the silkscreen.

UART Interface

Baud rate:

  • ZED-F9P: 9600-921600 bps
  • ZED-X20P: 4800-8000000 bps

Notes: Default baud rate is 38400 bps. The ZED-F9P only supports the RTCM protocol up to v3.3

SPI Interface

Max transfer rate:

  • ZED-F9P: 125 kB/s
  • ZED-X20P: 880-950 kB/s

Max clock speed:

  • ZED-F9P: 5.5 MHz
  • ZED-X20P: 7.25-12.8 MHz

Notes: The transfer rate for the ZED-X20P is based on the load capacitance. SPI interface must be enabled by the jumper.

I2C Interface

The ZED-F9P only supported I2C fast-mode; while the ZED-X20P supports standard mode, fast mode, and fast mode plus.

Max bit rate:

  • ZED-F9P: 400 kbit/s
  • ZED-X20P: 1000 kbit/s

USB Interface

While both boards provide a USB-C connection to the GNSS receiver, on the ZED-X20P we would advise users not to rely on this interface in their designs.

Notes: For the ZED-X20P, we broke out this interface as part of a preliminary design recommendation. However, u-blox has recently removed this interface from their latest datasheet. Therefore, we would recommend that users not integrate this interface into their future designs. Especially when it doesn’t support firmware updates.

Software Changes

Firmware Upgrade

As mentioned about the USB interface, above, it is only possible to perform firmware updates through the UART1 interface for the ZED-X20P.

Firmware upgrade through I2C (Qwiic) is possible, but is only for advanced users. You need (e.g.,) a Thing Plus board running a sketch to convert USB UART to I2C. Then you need to run the u-blox ubxfwupdate.exe from the command line with some special settings.

u-center Application

One of the biggest changes between the two GNSS receivers is the u-center software application. u-blox recommends their new u-center 2 software application for any GNSS engine, generation 10 or later.

Image of What's the Difference Between the ZED-F9P and the ZED-X20P

The first difference between the two applications is that users will notice is a required user account for u-center 2. While users will need internet access to initially login, users will not need internet access or to login afterwards.

Beyond a new look and feel, the primary difference in functionality between the two applications is that the new generation 10 GNSS engines implement a new set/get method for the values in the configuration layers of the GNSS receiver. This is handled in the backend of the software application, but should be noted for any development purposes.

Some other notes to mention:

  • With the new workspace configuration allows users to save setups and layouts when testing different GNSS receivers.
  • With the required login, u-blox also integrates their new PPP services and their support portal in the u-center 2 application for users.
  • u-blox also wrote up this blog post with a few tips and tricks for the new software application.

Notes: Nate has found that if users wish to continue using the original version of u-center (not u-center 2), they just need to use the generation 9 advanced configuration view. See Section 5.2.7 Generation 9 configuration view of this manual.

Arduino Library

With the introduction of the set/get method for configuration values for the gen 10 GNSS engines, our Arduino library got a new release (v3). The Arduino library should be mostly backwards compatible, with a few minor changes, see below for more information:

제조업체 부품 번호 GPS-28871
ALLBAND GNSS RTK BRKOUT XED-X20P
SparkFun Electronics
₩458,564
더 보기 Details
제조업체 부품 번호 16481
GPS-RTK-SMA ZED-F9P BREAKOUT
SparkFun Electronics
₩420,420
더 보기 Details
제조업체 부품 번호 15136
GPS-RTK2 BOARD - ZED-F9P (QWIIC)
SparkFun Electronics
₩420,420
더 보기 Details
제조업체 부품 번호 19032
SIK TELEMETRY RADIO V3 - 915MHZ,
SparkFun Electronics
₩260,370
더 보기 Details
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.