Maker.io main logo

Simple ESP32 CAM Object detection using Open CV

1,411

2024-09-09 | By Mirko Pavleski

License: General Public License Arduino ESP32 Adafruit Feather

Object detection is a computer vision technique that involves identifying and locating objects within an image or video. It is a fundamental task in various applications, such as surveillance, autonomous driving, and image retrieval. This time I will explain to you how to make a powerful object detection device that uses only an inexpensive ESP32 Camera module with a built-in FTDI USB to serial converter.

ui0

This means that there is no need for any soldering or connection of external components. We only need to connect the Module directly to the USB port of the PC. The whole system consists of two parts - Esp32 camera module with Arduino code installed - and the second part is а pc software, actually Python code that uses Open CV, which is a powerful library for computer vision tasks, including identifying and localizing objects, as well as object detection. In our case are processed series of images received from the camera module.

 

Now I will explain the installation method in order. First, we need to enable camera module support in the Arduino environment. For this purpose, we go to Arduino IDE - File - Preferences - where we add the ESP32 URL to "Board Manager URLs" as follows:(https://raw.githubusercontent.com/espressif/arduino-esp32/gh-pages/package_esp32_index.json)

kjl

Now click "Tool-->Board-->Board Manager", and search for "esp32". It is recommended to install version 2.0.6 or newer ESP32 core. I installed the latest version.

sdtr

Next, on Arduino IDE -> Tools -> ESP32 Arduino we choose: AI Thinker ESP32-Cam

ftugfyu

With this, the procedure for entering support for the specific camera module in the Arduino IDE is completed. Next, we install the ESP32cam library from the attached .zip file. We go to Sketch - Include Library - add ZIP library and select the given library.

hgjkgh

After this, we upload the provided Arduino code. Just don't forget to enter the credentials of our Wi-Fi network beforehand in the code. Now in the Arduino Serial Monitor we check if the camera is initialized and working, and we also need to remember the IP address that was assigned to it in the local network because we will need it when starting the Python code.

bhkmh

Next comes the installation of the Python environment section. For this purpose, we go to the Python page, download the latest version, and install it with default settings, noting that we need to mark the checkbox "add python .exe to path".

hjolji

As I mentioned at the beginning, in order for Python code to work, several necessary libraries need to be installed, namely NumPy, OpenCV, and cvlib libraries. For this purpose, we go to the command prompt and execute the following commands-type: pip install numpy and press enter. After the installation is done:

-type: pip install opencv-python and press enter

-type: pip install cvlib and press enter

hjklui

Now we start the Python IDLE editor which is an integral part of the Python installation, or any other Python editor. We go to File - Open - and search for the provided Python code. Let me mention that together with the code, there are three more files that must be located in the same folder as the code. When we open the code, we need to enter the IP address from the camera that was previously given to the Arduino Serial Monitor.

bvgxcfg

We press RUN, and if we have completed the previous steps, a video from the camera appears on the screen for a few moments, on which various objects surrounded by a rectangular green frame are detected. The name of the detected object is written on the upper part of the frame. And now let's see how it looks in real conditions. As can be seen from the examples, the system is capable of detecting objects with high precision.

gvhj

In particular, this system uses a pre-trained object detection model. The file "coco.names" contains the names of the 90+ objects that the YOLOv3 model is trained to detect. And finally, a short conclusion. Object detection has uses in almost all sorts of industries. It is used for tracking objects, people counting, automated CCTV surveillance, vehicle detection, etc. This is certainly the simplest and cheapest object detection system that can serve perfectly for the presentation of the possibilities of this technology, and for powerful object detection and identification even without using the Python Code we can use the AMB82-Mini IoT AI Camera, which will probably be the subject of analysis in one of my next videos.

Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.