Maker.io main logo

Rock'em Sock'em Robots - Part 4

56

2024-06-21 | By Zach Hipps

License: See Original Project Arduino

Over the last several months, I've been building my own version of the classic toy Rock ‎‎‘Em Sock ‘Em Robots. Because I like to overcomplicate and overengineer everything I ‎do, I decided to make mine life-size and controlled by pneumatic cylinders connected ‎to an air compressor. I invited my friend Will over because this game requires two ‎people to play. Before we can have our fighting robot face-off, there are a few things ‎that I need to finish first.‎

robot_1

 

In part two of this series, I built a simple control board for Red Robot. This board allows ‎me to connect two buttons and three solenoids. I went ahead and used a prototype ‎board because it's quick and easy, but now I need to build another for Blue Robot. ‎There are six solenoids in total, and each solenoid is going to need a MOSFET, a diode, ‎and several other passive components. That's going to get very overwhelming for a ‎prototype board like this. Not to mention, each robot is getting an inertial measurement ‎unit (the accelerometer and gyroscope). Finally, each robot is also going to have LED ‎bar eyes. That will be a lot of work to build on a prototype board. I think it's in my best ‎interest to design a custom PCB. If I tried to cram all of this on a prototype board, it ‎would introduce the possibility of so many problems. Whereas a PCB will be a lot more ‎reliable, and should any issues arise, it'll be easier to diagnose and troubleshoot those ‎problems.

board_2

board_3

board_4

This circuit board is straightforward because it has a lot of repeating components. I ‎design one solenoid driver circuit, and then I can just copy it six times. The same goes ‎for the button inputs. I can design the low pass filter and then just make a copy of it ‎four times. Once the boards arrive, I use the stencil to apply solder paste, then hand-‎place each component, and reflow them on my little hotplate. The finished circuit board ‎is divided in half. All the connectors on one side of the board will control Red Robot, ‎while all the connectors on the other side will control Blue Robot. In the middle, there’s ‎an Arduino Nano microcontroller, which reads all of the button inputs and controls the ‎solenoid outputs. I'm using a barrel jack to supply 12 volts to the solenoid valves. I also ‎have a dedicated set of connectors for the LED bar eyes and the IMU sensor. This ‎control board will sit between the two robots in the same place as the pneumatic control ‎valves. Connecting all six solenoid valves will be simple because they're close.‎

scheme_5

board_6

board_7

board_8

I don't want the arcade-style buttons that the players need to press to be in the center. ‎I'm trying to imagine myself playing this fighting robot game, and for me, it makes sense ‎for each player to stand behind their robot as they're operating their robot. I designed ‎and printed this little button grip, and I’ll wire in the arcade buttons and then attach the ‎grip to the skeleton frame. To do that I need to remove the skins, install the button grips ‎and mounts, and then replace the skins.‎

buttons_9

buttons_10

buttons_11

The next thing I do is install the small IMU. That's the inertial measurement unit, and it ‎sits inside the chest and will detect when the robot is being punched. Each of the ‎robots will have one of these IMUs. The sensor data will be fed into the central ‎microcontroller, and that microcontroller will also be reading the button pushes, as well ‎as sending out the LED information for the eyes in each of the robots.‎

imu_12

Here are the bar LEDs for the eyes. It is just ten regular LEDs all in one package, with ‎all the anodes on one side and all the cathodes on the other. To drive this, I'm using a ‎couple of shift registers. I need two of them because the shift registers that I have are ‎only eight bits, and I have ten LEDs, which is a bit silly to use an entire shift register ‎just for the last two LEDs, but that's what I end up doing.‎

leds_13

To make this a really clean install, I designed a little circuit board with the two shift ‎registers and a little connector that I will use for data and power. Unfortunately, the ‎solder pads for the shift registers are barely too wide to fit under the bar LED. So, I have ‎to get a little creative, and I place it on the other side of the PCB and make them ‎surface-mount solder pads. The problem is that this is a through-hole component! I'm ‎going to have to bend these leads over and make it a DIY surface mount part. I'll admit ‎that this is a janky solution, but I think it's going to work. To assemble this board, I first ‎solder on the current limiting resistors for the LEDs, and then I solder on the shift ‎register and the connector. Finally, I solder on the bar LED.‎

install_14

install_15

install_16

At this point, I connect the bar LED to the Arduino Nano and write some test code to ‎see if I can cycle through all the LEDs, but this is where I run into a problem. While ‎most of the LEDs are lighting up just fine, the 7th and the 10th LEDs are not ‎illuminating. I've got to troubleshoot that. I worry that I made a mistake on the circuit ‎board design and that when I plugged it in, it may have burned out those LEDs. Let’s ‎hope that's not the problem! I test each individual LED by applying 1.7V across each ‎individually. When I do that, it looks like both the problem LEDs light up just fine, and I ‎am relieved that I didn't burn those out. But I still have the problem that they're not ‎lighting up. I start looking at my schematic a little bit closer as well as my code, but ‎neither appear to contain the problem. I did some more digging, and it turns out that I ‎didn't make a mistake on the circuit board per se, but some of the LEDs used a thin 5V ‎trace around the edge of the board. It turns out that on the first board I built, I damaged ‎that 5V trace, so it wasn't intact. Therefore, those LEDs weren't getting the five volts that ‎they needed. Fortunately, I ordered enough parts to build more boards, so the solution ‎meant I just needed to build another board. I also took the time to build two blue bar ‎LEDs for the other robot. When I ran the test code on all these bar LEDs everything ‎was working great so now it's time to install them onto the robots.

testcode_17

testcode_18

testcode_19

testcode_20

testcode_21

testcode_22

testcode_23

testcode_24

testcode_25

testcode_26

testcode_27

I want to move the robots to the front yard for the fight, and I don't have a great way to ‎move them. I put them on a sheet of OSB and try to tug it along with the lawnmower, ‎like on a little raft, but it's pretty top-heavy, so I asked my wife to help stabilize it.‎

move_28

move_29

Round 1 (Zach 0 | Will 0)‎

It’s time to fight. Will has arrived, and we are both at the controls…Will is on Red Bot, ‎and I am on Blue Bot. Okay, Ready? Let's go! It is a quick fight with some fast punches ‎that ultimately knock out Blue Bot. Will is ahead 1-0.‎

fight_30

fight_31

fight_32

Round 2 (Zach 0 | Will 1)‎

We have Will with one win, and me with zero. The Red Bot must have an advantage, ‎so let’s switch sides and do best two out of three. All right, Ready? Uh oh… something ‎is not right. Red Bot’s right arm is not working. We discover that the arm wasn't even ‎attached during the first fight! As we were setting up, I found a little bolt on the table ‎and thought, “That's probably not a good sign”, but I didn't think any more about it and I ‎threw it in my pocket. It turns out this little bolt was holding the right arm on Red Robot! ‎Somehow Will beat me with only one working robot arm! Maybe in the next round, we ‎need to tie one of Will's arms behind his back. After a quick repair, it is time for my ‎redemption. Will tells me he’s feeling a quick, clean sweep right here. All right. Three, ‎two, one… Go!‎

Right hook right there. Right hook! Jab! I don't know any boxing terms, but it seems like ‎this round is going much better for me. The LEDs are getting knocked down, and I ‎have Will down to only one LED remaining! One more hit, and he’s gone. Out of ‎nowhere, my robot’s head pops up!!! Will sneaks in another win! Will is ahead 2-0. I ‎guess Will won two out of three already. That's really embarrassing. I have got to ‎redeem myself. Let’s play one more round because we are both having way too much ‎fun.‎

fun_33

fun_34

Round 3 (Zach 0 | Will 2)‎

Three, two, one. Go! I don’t stand a chance, and Will swiftly and expertly puts me out of ‎my misery, and my bot’s head pops up yet again! It is over. Will wins a clean sweep. ‎Will 3, Zach 0.‎

sweep_35

This project has been super fun to dream up and build. As I complete this project for ‎now, I have some thoughts. I was tempted to put in a microcontroller that could connect ‎to the Internet and play with somebody where they could be pushing the buttons on their ‎keyboard remotely and play as Red Robot, and I could be playing Blue Robot. The ‎problem, though, is latency. Between pushing a button on their keyboard, it has to be ‎transmitted over the internet before it would result in any movement of the robot arm. It ‎would be probably a half-second delay at best. Whereas my buttons are being read in ‎real time, and it wouldn't be a fair fight. So that's one of the reasons I decided against ‎doing that. Another fun option, which is more possible, would be to write a program ‎and have them be synchronized and do a synchronized robot dance. What do you ‎think? What should I do next with this ridiculous project?

제조업체 부품 번호 A000005
ARDUINO NANO ATMEGA328 EVAL BRD
Arduino
₩39,691
더 보기 Details
제조업체 부품 번호 09339
SWITCH PUSHBUTTON SPDT 3A 120V
SparkFun Electronics
₩5,498
더 보기 Details
제조업체 부품 번호 4646
9-DOF ABSOLUTE ORIENTATION IMU F
Adafruit Industries LLC
₩46,255
더 보기 Details
제조업체 부품 번호 LTA-1000HR
LED CBI 5.08X1.78MM 10SEG R VERT
Lite-On Inc.
₩1,699
더 보기 Details
제조업체 부품 번호 XGCBDX10D
LED CBI 5.08X1.78MM 10SEG BLU TH
SunLED
₩6,239
더 보기 Details
제조업체 부품 번호 4948
MINI HOT PLATE PREHEATER WITH US
Adafruit Industries LLC
₩192,957
더 보기 Details
Add all DigiKey Parts to Cart
Have questions or comments? Continue the conversation on TechForum, DigiKey's online community and technical resource.