New Product Discoveries - EPC's eGaN® FET Series GaNFET and Murata's Micro DC-to-DC Converter

In this episode of Digi-Key Electronics New Product Discoveries I explore some awesome, miniaturized components from EPC and Murata.

The first product I want to address is a GaNFET (Gallium Nitride Transistor), which is part of the Generation 5 eGaN FET series from Efficient Power Conversion (EPC). An important fact to understand is that, while most people have a model for how electricity flows “through copper,” in reality electricity moves over copper as a wave. The eGaN FET takes advantage of this principle by conducting current over the device as opposed to through it by means of surface mode conduction. In the end, what this means for a designer is that the component does not heat up. These components are perfect for achieving high current density in power supply and RF applications.

Another device I want to discuss is a DC-to-DC converter from Murata. The LXDC2HL series comes in an incredibly small package that takes in around 2 to 5 V and outputs a variety of regulated voltages. By virtue of Murata’s ferrite material, this product has very low Electromagnetic Radiation (EMR), so it has low noise in a very small package.

These awesome products are available on digikey.com. Thanks for watching!

작성자 정보

Image of Randy Restle

Randall Restle은 전자 부품 업계에서 40년 넘게 경력을 쌓아왔습니다. 현재 현직에서는 은퇴했으며, DigiKey에서 응용 분야 엔지니어링 부문 부사장을 역임했습니다. 숙련된 응용 분야 엔지니어, 기술자 및 관리 인력으로 구성된 팀을 이끌며 독창적이고 고유한 고급 기술 제품을 개발하도록 하는 등의 직무를 수행했습니다.

개인적으로 관심 있는 분야로는 디지털 신호 처리, 프로그래밍 가능한 로직 구현, 동작 제어 개선 및 소프트웨어 설계 등이 있습니다. 다양한 업계에 걸쳐 특허를 보유하고 있으며, IEEE의 수석 회원입니다. Randall은 신시내티 대학에서 BSEE, MS, MBA 학위를 취득했습니다.

More posts by Randall Restle
 TechForum

Have questions or comments? Continue the conversation on TechForum, Digi-Key's online community and technical resource.

Visit TechForum