Blast from the Past...

I recently had to venture up into my attic to solve a bathroom vent problem and rediscovered my stored away box of electronics covered in insulation and dust. Scraping it off and taking it down to my lab for inspection, I realized what I had forgotten about…

Dating myself here, but the days of getting into microprocessors back in 1983 and hacking my old CoCo computer (formerly known as The Color Computer which originally had 4k but I upgraded it to 16K ☺, LOL), came alive again when I opened the box. It brought out the exciting adventure of making an actual computer board using the old Motorola 6809, learning assembly language, and using wire wrap pins and a perf board to create it.

Soldering a ribbon cable to the mother board under the card edge connector gave me access to the port’s i/o lines for my computer board. I wrote assembly language in a program called EDTASM and used a 5 ¼ inch floppy disk drive to run the program. Using a programmer board to burn in my assembled program to an EPROM, I then inserted it to the computer board for testing where I experimented with stepper motors to run a homemade plotter.

As technology and the embedded world evolved, things kept getting better. I was hired by DigiKey in 1984 to support a popular item called the DB10 board, which was a tiny basic computer board from National Semiconductor that used a CRT (cathode ray tube or terminal which resembled a small TV) and keyboard to write basic programming language where you could easily get to the peripheral adapter ICs and output to a transistor driver for driving stepper motors, lighting LEDs, or sending a message to a LCD dot matrix display.

Excerpt from DigiKey catalog

Again, as technology evolved, the microcontroller was created. It basically combined all areas of a microprocessor system - i.e., microprocessor, address decoding, static memory, program memory, peripheral interface adapter ICs, oscillator, and capacitors.

Excerpt from DigiKey catalog

In the early 90s we added the PIC line of microcontrollers with an inexpensive programmer from Parallax Inc (at that time it was the lowest cost programmer for our customers). Appearing in over 6 million catalogs mailed out, this unique combination skyrocketed sales of MCUs and the revolution began. Since then and today we’ve added a ton of development boards (product index) and MCU suppliers. Arduino, Raspberry PI, and Beagle Bone, to name a few, have all been very popular with our customers.  To make finding boards easier, we created the Development Tools Product Selector guide.

When you think about how technology has evolved from the first fax machine, the internet, microprocessor to microcontroller, cell phones, IoT, 3D printing and artificial intelligence, you must ask: what will be next in the evolution of these exciting times…a Star Trek like transporter or revealing an alien contact?

 

작성자 정보

Image of John LeDuc

DigiKey의 디지털 사업부 프로젝트 관리자인 John LeDuc는 1984년부터 DigiKey 고객의 기술 관련 질문을 처리하고 제품을 검토하여 카탈로그에 추가하는 작업을 해왔습니다. John LeDuc는 National Semiconductor의 INS8073 Tiny Basic 데모 기판 지원을 전문으로 했으며, 현재는 당사 웹 사이트 개선을 위한 우수한 아이디어를 취합하고 생성하여 엔지니어링 고객에게 더 나은 디지털 경험을 제공하는 일을 하고 있습니다. John은 Electronics Technology에서 준학사 학위를 취득했으며 여가 시간에 전자 장치를 조작하고 3D 프린터로 고유한 설계을 만드는 '밤의 엔지니어'이기도 합니다.

More posts by John LeDuc
 TechForum

Have questions or comments? Continue the conversation on TechForum, Digi-Key's online community and technical resource.

Visit TechForum