Why Bigger is Better When it Comes to Drones

Drones come in all sizes—from very big to very small. One would think that the larger, heavier drones would have shorter flight times, right? Surprisingly that is not the case, according to Rhett Allain from Wired Magazine. Rhett did some research on the physics behind why bigger drones can fly longer.

If you want to take a deep look at the physics of drones, you can read how varying the power to four rotors allows the vehicle to fly in every different way. I also looked at the power needed to hover using very basic physics models—a question that actually started with my estimation of the power needed for the SHIELD helicarrier to fly (it's huge).

Let's recap how I can estimate the power need to hover a drone. Imagine you have a drone with spinning rotors. It actually doesn't matter if you have just one rotor (like a helicopter) or four like a quadcopter or even eight like an octocopter. What really matters is that the rotors take stationary air above the vehicle and push this air down.

Now for the fun stuff. Let's look at the battery size and power for two drones.

These small drones have to save mass for other important stuff that just can't get any smaller. The sacrifice for small drones is a short flight time—at least for now.

Read the complete article on Wired to take a deeper dive into how Rhett came up with his conclusions. It’s pretty interesting and worth a look.

작성자 정보

Image of Jenn Toso

소셜 미디어 마케팅 전문가인 Jenn Toso는 소셜과 관련된 모든 것을 전문으로 합니다. 그녀는 DigiKey의 소셜 미디어팀의 헌신적인 구성원이며 DigiKey의 소셜 미디어 채널에서 그녀의 블로그, 공유, 트위트, 게시물을 볼 수 있습니다. Jenn은 메이커 및 STEM 커뮤니티에 열정적으로 참여하고 있으며 오늘날의 젋은이들이 모두의 밝은 내일을 위한 키를 쥐고 있다고 믿습니다. Jenn은 경영학 학사, 인터넷 마키팅 석사를 획득했으며 하키맘으로서는 박사입니다. 여유 시간에는 새롭운 관심사인 웨어러블 기술에 대해 탐색하기를 즐기거나 하키에 대한 열정을 불태웁니다. 일부 유형의 소셜 미디어나 아이스하키 경기장에서 또는 둘 모두를 동시에 즐기는 Jenn을 쉽게 찾을 수 있습니다.

More posts by Jenn Toso
 TechForum

Have questions or comments? Continue the conversation on TechForum, Digi-Key's online community and technical resource.

Visit TechForum