Toy Teaches Kids Braille in Fun, Simple, and Affordable Way

BecDot is a toy that also doubles as a learning tool. Not only is it fun to play with but it also teaches braille. Braille is an essential skill for children with visual impairments to have so that they can keep up with their peers—both socially and academically.

BecDot came about because a father was not satisfied with the braille tools that were currently available for his daughter, so he decided to get to work and design his own!

One of the things holding back devices like this is the complexity and cost of braille displays. If you think what’s behind an LCD is complicated, imagine if every pixel needed to actually move up and down independently and withstand frequent handling. The braille equivalents of e-readers can cost thousands to display a sentence or two at a time — but of course kids don’t need that.

Unsatisfied with the available options, Jake decided to engineer his own. He created a simple Scotch yoke mechanism that can control up to three dots at a time, meaning two of them can create a braille letter. It’s all controlled by an Arduino Uno. Simple means cheap, and the other parts are far from expensive; he told me that his bill of materials right now is around $50, and he could probably get it below $30.

Read more about how the BecDot was made in TechCrunch:  http://dky.bz/2G6r8aS

작성자 정보

Image of Jenn Toso

소셜 미디어 마케팅 전문가인 Jenn Toso는 소셜과 관련된 모든 것을 전문으로 합니다. 그녀는 DigiKey의 소셜 미디어팀의 헌신적인 구성원이며 DigiKey의 소셜 미디어 채널에서 그녀의 블로그, 공유, 트위트, 게시물을 볼 수 있습니다. Jenn은 메이커 및 STEM 커뮤니티에 열정적으로 참여하고 있으며 오늘날의 젋은이들이 모두의 밝은 내일을 위한 키를 쥐고 있다고 믿습니다. Jenn은 경영학 학사, 인터넷 마키팅 석사를 획득했으며 하키맘으로서는 박사입니다. 여유 시간에는 새롭운 관심사인 웨어러블 기술에 대해 탐색하기를 즐기거나 하키에 대한 열정을 불태웁니다. 일부 유형의 소셜 미디어나 아이스하키 경기장에서 또는 둘 모두를 동시에 즐기는 Jenn을 쉽게 찾을 수 있습니다.

More posts by Jenn Toso
 TechForum

Have questions or comments? Continue the conversation on TechForum, Digi-Key's online community and technical resource.

Visit TechForum