All the Internet of Things: Episode One Recap

Have you had a chance to watch the first episode of Adafruit and DigiKey’s “All the Internet of Things”? Presented by Lady Ada herself, the series “All the Internet of Things” is covering everything you need to know about the IoT. The second episode is scheduled to release shortly, and, with that, a quick review of the first episode will prepare you for the next release.

Episode one is devoted to Transports (the different standards and associated protocols) that enable the IoT. In this episode she discusses the pros and cons of Ethernet, WiFi, Bluetooth and BTLE, Cellular and Satellite, Zigbee and Z-Wave, as well as LoRa and SigFox. The full video is almost 40 minutes, but conveniently, Adafruit has also broken down the video into a step-by-step walk though for each topic.

If you are looking for information on only one topic or simply don’t have the time to watch the whole video at one time, these smaller segments may be just what you’re looking for so you can on what you are most interested in:

Ethernet (about 4 minutes)

WiFi (about 7 minutes)

Bluetooth & BTLE (about 7 minutes)

Cellular & Satellite (about 6 minutes)

Zigbee & Z-Wave (about 4 minutes)

LoRa & SigFox (about 2 minutes)

The full length video is available on maker.io, as well.

작성자 정보

Image of Jeff Zbacnik, Jr., DigiKey

Jeff Zbacnik, Jr.는 DigiKey의 숙련된 전자 기술자입니다. 2003년부터 DigiKey에서 근무한 Jeff Zbacnik는 제품 리뷰, 비평, 기발한 상품 개발(점멸 LED)을 전문으로 합니다. DigiKey Scholarship 프로그램이 시작된 해에 노스랜드 커뮤니티 및 테크니컬 컬리지에서 전기 기술 부분 응용 과학 준학사 학위를 받았습니다. 항상 Playstation 게임을 하고 있거나 게임을 생각하고 있는 Playstation 게임 매니아입니다.

More posts by Jeff Zbacnik, Jr.
 TechForum

Have questions or comments? Continue the conversation on TechForum, Digi-Key's online community and technical resource.

Visit TechForum