The Significance of the Intrinsic Body Diodes Inside MOSFETs
DigiKey 제공
2016-09-22
Figure 1 shows a cross-section of an N-channel enhancement-mode MOSFET with the intrinsic body diodes indicated symbolically. These MOSFETs have diodes in them pointing from the body to the drain and source. The body to source diode is usually irrelevant, because it is shorted out by an internal body to source connection.
These diodes are appropriately named body diodes, and with the exception of JFETs, they are intrinsic to any FET type. There are P-N junctions in the FET structure between the substrate and the doped regions.
Current typically flows from the drain to the source in N-channel FET applications because of the body diode polarity. Even if a channel has not been induced, current can still flow from the source to the drain via the shorted source to body connection and the body to drain diode. Because of this, a typical N-channel FET cannot block current flow from its source to its drain.
In some applications, such as certain DC-to-DC converters, the body diode is actually relied upon for normal circuit operation. In contrast, it doubles the number of FETs necessary in other applications, such as certain power source selectors, where current must be blocked in both directions.
The two back-to-back P-N junctions also result in an intrinsic BJT (Bipolar Junction Transistor) within the FET; however, with a shorted body to source connection it effectively ceases to exist.
More considerations regarding MOSFET construction and operation are available here.

Figure 1: Cross-section of an N-channel enhancement-mode MOSFET with the intrinsic body diodes indicated symbolically.
면책 조항: 이 웹 사이트에서 여러 작성자 및/또는 포럼 참가자가 명시한 의견, 생각 및 견해는 DigiKey의 의견, 생각 및 견해 또는 DigiKey의 공식 정책과 관련이 없습니다.