Software-Defined Radio Advanced RF Transceiver

작성자: Analog Devices, Inc.

DigiKey 제공


The astonishing, sometimes bewildering array of available wireless standards, with their different frequencies, bandwidths, protocols, and formats, has given users unprecedented connectivity and access. However, it has also meant that engineers of wireless systems are faced with severe challenges when designing or investigating issues, performance, and options.

The solution seems obvious: minimize use of dedicated hardware, and instead rely on a software-defined radio (SDR) to implement and manage as much of the transmitting and receiving functionality as possible. Today's high-performance, low-power processors, including FPGAs, and their ability to execute complicated algorithms at high speed make such real-time implementation practical.

However, there is a real-world impediment to this solution: it is difficult to design wideband analog circuitry for the receiver and transmitter signal paths. As a result, most broadband SDRs use a set of overlapping, parallel analog channels, each optimized for a specific slice of the overall band, and with bandwidths matched to the signals of interest in each segment. While this approach is technically effective, it requires considerable hardware, PC board real estate, power, and, of course, cost.

That is the dilemma which Epiq Solutions (Schaumburg, IL 60173), faced as they developed their latest SDR unit, the Maveriq™ Multichannel Reconfigurable RF Transceiver, (Figure 1) an advanced platform combining multiple RF transceivers, internal solid-state drive (SSD) for data recording, an on-board Intel x86 CPU running Linux, and a gigabit Ethernet interface for high-speed data access. As designers and builders of state-of-the-art, reconfigurable radio systems for mission-critical applications, their objective was to deliver a more powerful multi-channel version of their existing Matchstiq™ SDR.

Image of Maveriq™ Multichannel Reconfigurable RF Transceiver from Epiq Solutions

Figure 1: The Maveriq™ Multichannel Reconfigurable RF Transceiver from Epiq Solutions offers significant SDR capability in a small package, and covers a tuning range from 100 MHz to 6 GHz.

Despite its advanced features and capabilities, Maveriq is a portable, low-power platform; while previous solutions required large and bulky hardware configurations. Combined with a library of ready-to-run specialty software applications, Maveriq can immediately be used to solve challenging signal-processing requirements. These include scanning and decoding cellular radio signals from both basestations and mobile phones; recording wideband RF to its internal hard drive (SSD) as well as RF playback; and implementing 2 × 2 MIMO (multiple input, multiple output) waveforms.

An IC enables a new design approach

What allowed the engineers at Epiq to pack this much performance into a small, low-power unit was the availability of a new IC, the AD9361 RF Agile Transceiver from Analog Devices, specifically tailored for SDR applications. According to John Orlando, Epiq's CEO and System Architect, "The AD9361 provides the RF flexibility and integration needed to enable our next-generation SDR platform." Watch the AD9361 RF Transceiver and Support Ecosystem video which provides a short overview of the product.

This 10 mm × 10 mm chip-scale device with dual independent channels (Figure 2) has user-tunable bandwidth from 200 kHz to 56 MHz, and 12-bit A/D and D/A converters operating up to 61.44 MSPS, along with other features and performance which are needed to build a signal chain spanning 70 MHz to 6 GHz. Critical operating parameters are user-adjustable "on the fly" for optimum matching to the application requirements. Using this component reduced the overall footprint of the entire analog front-end (AFE) while keeping power consumption for this portion of the design in the 1 W region, essential to stay within the product power budget.

Image of Analog Devices' AD9361 RF Agile Transceiver IC

Figure 2: Analog Devices' AD9361 RF Agile Transceiver IC integrates the many RF functions needed for a 2 x 2 analog signal chain while allowing user programmability; thus greatly minimizing board space, power consumption, and cost.

The overall Maveriq unit (Figure 3) supports 2 × 2 MIMO or 4-channel receiver configurations via a pair of AD9361s, with an RF tuning range from 100 MHz to 6 GHz, 1 kHz step size, and 2 ms tuning time. It includes an integrated GPS receiver with 1 PPS performance, up to a 1 TB internal solid-state hard drive (SSD) supporting data recording 100+ MB/s (sustained), and Gigabit Ethernet for interfacing to external systems.

Image of Epiq Maveriq™ block diagram

Figure 3: The Maveriq unit comprises RF, baseband, processing, storage, and connectivity functions with much more detail and sophistication than this basic block diagram can reveal.

The processing function is centered on a dual-core Intel x86 CPU running Linux, plus an FPGA for signal-processing tasks, along with run-time loadable/executable software applications, all supported by an available software-development kit (SDK) for custom applications. The entire unit is just 9.1” × 6.6” × 1.7” (23 × 16.7 × 4.3 cm), weighs 1.9 lbs (0.9 kg), and dissipates 15 W (depending on FPGA and I/O usage).

Of course, processing power is inadequate without suitable RF performance. The receiver has a typical noise figure of less than 8 dB and typical IIP3 of -10 dBm. Transmit-side performance parameters such as bandwidth, tuning, and speed complement the receive-side numbers, along with output power of +5 dBm.

Although the AD9361 IC was a key enabler for this design, additional improvements are always on the horizon. Certain applications require stretching the RF performance down to the 20 MHz range and below, which is beyond the reach of the AD9361. Further, selection of RF components such as low-noise amplifiers (LNAs) capable of operating down to 20 MHz can also be a challenge, especially for size and power-constrained designs. It is simplistic to think that advances in low-power processing coupled with availability of large amounts of memory plus high-speed digital I/O and connectivity, all driven by Moore's law, are sufficient for a viable small, high-performance SDR. The reality is that the front-end channel for both receive and transmit paths is just as important, and developments in RF ICs which combine analog processing, filtering, and conversion not only minimize the algorithm burden, but make much of the actual SDR performance possible.

DigiKey logo

면책 조항: 이 웹 사이트에서 여러 작성자 및/또는 포럼 참가자가 명시한 의견, 생각 및 견해는 DigiKey의 의견, 생각 및 견해 또는 DigiKey의 공식 정책과 관련이 없습니다.

작성자 정보

Analog Devices, Inc.

게시자 정보

DigiKey

미네소타주 시프리버폴스에 위치한 DigiKey는 전자 부품의 시제품 제작/설계 및 양산 모두를 위한 세계적인 풀서비스를 제공하는 업체로서 DigiKey 웹사이트를 통해 750개 이상의 유수 제조업체에서 공급하는 600만 개 이상의 제품을 제공합니다.