Difficult Design Challenges Solved with 2 to 14 GHz Matched Microwave Mixer

작성자: Linear Technology

A new very wideband mixer with integrated LO (local oscillator) buffer and frequency doubler solves several challenging problems for microwave designers. The LTC5548 mixer from Linear Technology eases design with the following key features:

  • IF (intermediate frequency) port, extending from DC to 6 GHz, eases wideband IF sampling
  • On-chip LO limiting amplifier eliminates external LO buffer stage, reducing cost and minimizing total solution size compared to hybrid module solutions
  • 0 dBm LO drive reduces total radiation leakage, reducing external filter and shielding requirements
  • Ultra-wideband RF (2 to 13.6 GHz) and LO (1 to 12 GHz) ports are continuously matched

The device has a wideband differential IF port that works from DC to 6 GHz. Its low frequency capability makes for more flexible frequency planning. The LTC5548 is ideal for receiving wideband signals, especially with bandwidths of 500 MHz to 1 GHz or higher.

Unlike most microwave mixers, which typically require a hefty +13 dBm or higher LO drive, the LTC5548 has an integrated LO buffer and only requires 0 dBm drive. Since the device starts with a 0 dBm signal, rather than the +13 dBm or higher typical with alternative devices, the LO leakage present at other ports is 13 dB lower. This results in much simpler filtering requirements, especially with the low IF frequencies the LTC5548 can support. The on-chip LO buffer significantly improves the RF to LO port isolation, which helps reduce any issues with frequency pulling of the synthesizer source due to a parasitic RF signal at the LO input.

The LTC5548 is designed for wideband operation and can be used bidirectionally, either as an up-conversion or down-conversion mixer. Its RF port can be the input in a down-converting receiver or the output in an up-converting transmitter. Its RF port has an on-chip balun, enabling it to operate single-ended. The balun transformer is matched to 50 Ω continuously from 2 to 13.6 GHz, with better than 10 dB return loss.

To make the part truly useful for wideband applications, its LO port is also single-ended and is matched to 50 Ω continuously from 1 to 12 GHz. Additionally, the 50 Ω impedance termination is constant, regardless of whether the LTC5548 is enabled or disabled.  So switching the mixer on and off produces no disturbance that could unlock the phased-locked loop in the LO source.

The 50 Ω ports greatly ease design for the microwave system designer. First, this makes for simpler filtering and interfacing to other parts of a 50 Ω system. Secondly, the extremely broadband match is far more forgiving to the circuit’s sensitivity to external matching component value variations, producing very consistent performance with system production variations.

The LTC5548’s LO port can be driven directly with a signal source to 12 GHz for best noise figure and spur performance. Alternatively, the port can be configured to use the internal frequency doubler; when selected (via a digital select pin), up to a 6 GHz LO signal and double it internally to operate up to 12 GHz. This facilitates the use of a lower cost, low frequency PLL/synthesizer. The trade-off is a 3 dB increase in noise, primarily due to the doubling of the noise power, with slightly higher spurs.

Diagram of wideband 10 MHz to 6 GHz up-conversion to 6.5 GHz

Figure 1:  Wideband 10 MHz to 6 GHz up-conversion to 6.5 GHz.

The result is an extremely small size solution.  An example of a wideband transmitter application is shown in Figure 1. This circuit up-converts a 10 MHz to 6 GHz input signal, using a swept LO frequency of 6.51 to 12.5 GHz, thereby creating a fixed 6.5 GHz RF output. To achieve such wideband input performance, a Mini-Circuits model TCM1-83X+ balun transformer is used to convert the single-ended input to the differential IF port of the mixer. With high-side LO injection, the mixer exhibits a relatively flat conversion loss from near DC to 3 GHz, as shown in Figure 2. Within any 1 GHz of input bandwidth below 5 GHz, the gain flatness is better than 1 dB. Once the input is pushed above 5 GHz, the conversion loss begins to change more rapidly. The input IP3 (IIP3) remains greater than 23 dBm from near DC to 2.5 GHz, while still showing better than 19 dBm IIP3 up to 6 GHz.

Graph of conversion loss and IIP3 versus input frequency

Figure 2: Conversion loss and IIP3 versus input frequency using high-side LO drive and the LO drive.

The LTC5548 is built on an advanced SiGe BiCMOS process with very consistent performance. The mixer is housed in a tiny 2 mm x 3 mm plastic QFN package. With 0 dBm LO drive, the aforementioned example circuit implementation illustrates an extremely compact solution with minimal external components. The total solution cost is attractive, and an otherwise complex microwave circuit solution is made much simpler and more manufacturable.

Credit:  This article first appeared in the April 2016 issue of Microwave Journal as “2 to 14 GHz Matched Microwave Mixer Solves Difficult Design Challenges”

면책 조항: 이 웹 사이트에서 여러 작성자 및/또는 포럼 참가자가 명시한 의견, 생각 및 견해는 DigiKey의 의견, 생각 및 견해 또는 DigiKey의 공식 정책과 관련이 없습니다.

작성자 정보

Linear Technology