A Basic Guide to USB

작성자: Ashley Awalt

DigiKey 제공

What is USB (Universal Serial Bus)? USBs are rectangular-shaped connectors used for data transfer and power administration. They are most commonly used for charging devices or transferring data from a storage device to a viewing device. USBs were originally created to help simplify the connection of computers with peripheral devices.

The female connector (receptacle) is typically embedded into a device while the male connector (plug) is generally free-hanging so it can be placed on the end of a cable assembly for two or more devices to be interconnected at a time.

USB versions

USB 1.0 was introduced in 1996. Not many were utilized in new products until 1998 when USB 1.1 was released. This version only included standard A and B type connectors. At this point, with a speed of 12 Mbit/s, USB 1.1 was becoming more widely adopted.

USB 2.0 boasted a speed of 480 Mbit/s when it was released in 2000, the same year the Mini-A and Mini-B connector types were released. After many upgrades and improvements, including battery charging capabilities, the Micro USB connector type was released in 2007.

USB 3.0, released in 2008, also came with the new SuperSpeed transfer mode that reached a signaling rate of 5 Gbit/s. The SuperSpeed connectors are marked with a special logo while the standard receptacles have blue inserts to help identify those capabilities.

USB 3.1 was revealed in 2013 to upgrade the speed to 10 Gbit/s, thus passing the original SuperSpeed transfer mode. The new logo to distinguish this from the old SuperSpeed is SUPERSPEED+. In 2014 USB C was released under this specification.

USB 3.2 was released in 2017 and includes the specifications of all previous 3.X connectors, while offering up to 20 Gbit/s data rates and two-lane operation.

USB4 was the first USB protocol made strictly for USB C and became available in 2019. With this new generation came a new nomenclature as it no longer included a space after USB. As far as technical upgrades, it is based on the Thunderbolt 3 protocol developed by Intel and Apple. It can offer up to 40 Gbit/s.

USB4 2.0 was released in 2022 and can provide up to 80 Gbit/s bidirectionally and 120 Gbit/s asymmetrically.

Connector types

There are quite a few styles of USB connectors; the images and descriptions below will go over the most common types.

Type A (Figure 1): This is the most commonly utilized USB style. It is found in a multitude of places such as: computers, flash drives, cars, wall converters, etc. This type has four contact points, two for data and two for negative and positive power. They are all positioned alongside each other. 

Image of male/plug and female/receptacle USB Type A connectors

Figure 1: Male and female USB Type A connectors.

Type B (Figure 2): This style of USB was designed for peripheral device connection to computers. Peripheral device examples include keyboard, mouse, scanner, etc. This type has four contact points, just like Type A. Two are for data and two for negative and positive power. Two are positioned on the top, and two on the bottom.

Image of male/plug and female/receptacle USB Type B connectors

Figure 2: Male and female USB Type B connectors.

Type Mini A (Figure 3): This is not one of the more commonly used styles. This type has five contact points. All positioned in a straight line.

Image of male/plug and female/receptacle USB Type Mini A connectors

Figure 3: Male and female USB Type Mini A connectors.

Type Mini B (Figure 4): This style was previously used in cell phones for charging capabilities. This type has five contact points. All positioned in a straight line.

Image of male/plug and female/receptacle USB Type Mini B connectors

Figure 4: Male and female USB Type Mini B connectors.

Type Micro A (Figure 5): The Micro A is not as common as the Micro B. This type has five contact points. All positioned in a straight line.

Image of male/plug USB Type Micro A connector

Figure 5: Male USB Type Micro A connector.

Type Micro B (Figure 6): This style is very common. It is currently used for most major cell phone charging connectors. This type has five contact points. All positioned in a straight line.

Image of female/receptacle and male/plug USB Type Micro B connector

Figure 6: Female and male USB Type Micro B connector.

Micro B SuperSpeed (Figure 7): This is becoming more popular as it claims to have faster data transfer and charging rates. This type has 10 contact points, five in the standard Micro B portion and 5 in the additional portion. This receptacle is backwards compatible with all Micro B plugs.

Image of male/plug and female/receptacle USB Type Micro B SuperSpeed connectors

Figure 7: Male and female USB Type Micro B SuperSpeed connectors.

Type C (Figure 8): This style is reversible. It is starting to be utilized by certain phone companies due to claims of faster data and charging rates. This type has twenty-four contact points. Aside from the standard data transfer and power pins, this also has one configuration pin to determine the cable orientation.

Image of male/plug and female/receptacle USB Type C connectors

Figure 8: Male and female USB Type C connectors.

Looking for a specific USB cable assembly or connector? DigiKey has a wide variety to offer:

USB cable assemblies

USB connectors

USB adapters

References

  1. Wikipedia USB,” last modified February 7, 2017
  2. USB Connector Guide – Guide to USB Cables,” Cables To Go, accessed February 14, 2017,
DigiKey logo

면책 조항: 이 웹 사이트에서 여러 작성자 및/또는 포럼 참가자가 명시한 의견, 생각 및 견해는 DigiKey의 의견, 생각 및 견해 또는 DigiKey의 공식 정책과 관련이 없습니다.

작성자 정보

Image of Ashley Awalt

Ashley Awalt

Ashley Awalt는 2011년부터 응용 엔지니어링 기술 전문가로서 DigiKey에서 근무하고 있습니다. 그녀는 DigiKey의 장학금 프로그램을 통해 노스랜드 커뮤니티 및 테크니컬 컬리지에서 응용 과학 전문 학사 학위를 받았습니다. 그녀는 현재 고유한 기술 프로젝트를 생성하고, 공정을 문서화하며, 프로젝트에 대한 비디오 미디어 보도 제작에 참여하고 있습니다. 여가 시간에는 엄마로서 자녀들과 더 많은 시간을 함께 보내기 위해 노력합니다.

게시자 정보

DigiKey

미네소타주 시프리버폴스에 위치한 DigiKey는 전자 부품의 시제품 제작/설계 및 양산 모두를 위한 세계적인 풀서비스를 제공하는 업체로서 DigiKey 웹사이트를 통해 750개 이상의 유수 제조업체에서 공급하는 600만 개 이상의 제품을 제공합니다.