COMMAND SYNTAX <channel>:MoDulateWaVe<parameter>
<channel>:={C1, C2}
<parameter>:= {a parameter from the table below. }
Parameters Value Description
STATE <state> Turn on or off modulation. Note: if you want to
set or read other parameters of modulation, you
must set STATE to ON at first.
AM, SRC <src> AM signal source.
AM, MDSP <mod wave shape> AM modulation wave. Only when AM signal
source is set to INT, you can set the param
eter.
AM, FRQ <AM frequency> AM frequency. Only when AM signal source
is set to INT, you can set the parameter.
AM, DEPTH <depth> AM depth. Only when AM signal source is set to
INT, you can set the parameter.
DSBAM, SRC <src> DSBAM signal source.
DSBAM, MDSP <mod wave shape> DSBAM modulation wave. Only when AM signal
source is set to INT, you can set the parameter.
DSBAM, FRQ <DSB-AM frequency> DSBAM frequency. Only when AM signal source
is set to INT, you can set the parameter.
FM, SRC <src> FM signal source.
FM, MDSP <mod wave shape>
FM modulation wave. Only when FM signal
source is set to INT, you can set the parameter.
FM, FRQ <FM frequency> FM frequency. Only when FM signal source is set
to INT, you can set the parameter.
FM, DEVI
deviation >
FM frequency deviation. Only when FM signal
source is set to INT. you can set the parameter.
PM, SRC, <src> PM signal source.
PM, MDSP <mod wave shape> PM modulation wave. Only when PM signal
source is set to INT, you can set the parameter.
PM, FRQ <PM frequency> PM frequency. Only when PM signal source is set
to INT, you can set the parameter.
PWM, FRQ <PWM frequency>
PWM frequency. Only when carrier wave is
PULSE wave, you can set the parameter.
PWM, DEVI <PWM dev> Duty cycle deviation. Only when carrier wave is
PULSE wave, you can set the parameter.
PWM, MDSP <mod wave shape> PWM modulation wave. Only when carrier wave
is PULSE wave, you can set the parameter.
PWM, SRC <src> PWM signal source.
PM, DEVI <PM phase offset>
PM phase deviation. Only when PM signal
source is set to INT, you can set the parameter.
ASK, SRC <src> ASK signal source.